DDR validation has encountered a problem in codewarrior tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR validation has encountered a problem in codewarrior tool

4,365 Views
rameshasp
Contributor IV

When we are doing DDR validation test on LS1021A-TWR board using Codewarrior Licensed tool, getting below error message. Please provide your feedback.

rameshasp_0-1623410254230.png

 

0 Kudos
Reply
2 Replies

4,348 Views
ufedor
NXP Employee
NXP Employee

1) Do you really use TWR-LS1021A board?

2) Are you using CWH-CTP-CTX10-YE probe tip?

3) Please provide U-Boot booting log as text attachments and screenshot of the DDR Validation Tool Wizard containing parameters used for the validation.

0 Kudos
Reply

4,338 Views
rameshasp
Contributor IV

1) Do you really use TWR-LS1021A board?

Yes i am using TWR-LS1021A evk board.

2) Are you using CWH-CTP-CTX10-YE probe tip?

yes i am using CWH-CTP-CTX10-YE probe tip.

3) Please provide U-Boot booting log as text attachments and screenshot of the DDR Validation Tool Wizard containing parameters used for the validation.

Below attached the screenshot of TWR_LS1021A board Hardware connection and DDR validation tool containing parameters used for the DDR validation:

 

Could you please suggest why we are not able to complete DDR validation in EVK board, fyi, DDR validation is happening upto 12.03% after that diagnostic error is getting.

 

0 Kudos
Reply