Hi everyone,
We are working on a T1042 based Custom board. We have some differences when compared with RDB. We removed swithes which inditaces boot from where (NOR,NAND,SD).
What procedure should we follow when creating new PBL/RCW to change boot location using latest Code Warrior Flash programmer and QorIQ Suite together ? Is there any guide documentation ?
We are also open for other ideas.
Regards.
已解决! 转到解答。
> We removed swithes which inditaces boot from where (NOR,NAND,SD).
Please provide the processor connection schematics for inspection.
> creating new PBL/RCW to change boot location
Which boot source is planned to be used - refer to the QorIQ T1040 Reference Manual, 4.6.4.1 Reset configuration word (RCW) source.
> Please provide the processor connection schematics for inspection.
I am afraid but sharing is not applicable for me.
> Which boot source is planned to be used - refer to the QorIQ T1040 Reference Manual, 4.6.4.1 Reset configuration word (RCW) source.
This should be what I'm looking for. I'll only do 16 bit NOR flash booting. Does Code Warrior QCVS - RCW project have config variables to change these variables to generate new PBL ?
Thanks.