Connect LS2084 to FPGA without PHY.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connect LS2084 to FPGA without PHY.

Jump to solution
837 Views
miha_at_work
Contributor III

Hello.

I need do connect LS2084 to FPGA XC7A200T. I want to use high speed interfaces. I think to use PCI-Express or XAUI. But our programmers never worked with these interfaces. It is possible to use 10GBase-KR or 1000Base-KX without any external PHY? I saw no information about do I need or don't need it in reference manual or datasheet.

0 Kudos
1 Solution
689 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes it is possible to use 10GBase-KR or 1000Base-KX without any external PHY.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
690 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes it is possible to use 10GBase-KR or 1000Base-KX without any external PHY.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------