The documentation, below, on the RCW declares the variables for IRQ11_BASE to IRQ03_BASE to be 397 to 405 respectively.
However, in the LSDK-20.12 code for the LS1088 those values are shown in reverse order. The values IRQ03_BASE to IRQ11_BASE are 397 to 405 respectively.
https://source.codeaurora.org/external/qoriq/qoriq-components/rcw/tree/ls1088ardb/ls1088rdb.rcwi
The licensed Code Warrior we purchased for this processor states them the same as the LSDK.
Can anybody confirm through usage which set of values are correct.
In our experience the IRQ numbers are reversed. We have to switch IRQ06 with IRQ08 in order to get the IRQ to work. The IRQ_EXT value we set is all zeroes.
Please provide binary image of the RCW being used.
LSDK and CodeWarrior order is correct according to the internal documentation.
Please ensure that 378-376 IRQ_EXT is all zeroes.