I am working on PCI driver for LS1046ardb as root complex. For the configuration of the translation of target address to the address of PCI space, I need to know the lower base address of configuration space of PCI (which i did not get from the technical reference manual of LS1046ardb). Kindly provide me information about the Lower base address of Configuration spaces (Type 0 as well as Type 1) and the Outbound Mem/IO address spaces.
Regards.
This is a copy of the question: