Configuration Space Address of PCIe in LS1046ardb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuration Space Address of PCIe in LS1046ardb

977 Views
amnatehreem
Contributor II

I am working on PCI driver for LS1046ardb as root complex. For the configuration of the translation of target address to the address of PCI space, I need to know the lower base address of configuration space of PCI (which i did not get from the technical reference manual of LS1046ardb). Kindly provide me information about the Lower base address of Configuration spaces (Type 0 as well as Type 1) and the Outbound Mem/IO address spaces.

Regards.

Labels (1)
0 Kudos
1 Reply

721 Views
ufedor
NXP Employee
NXP Employee

This is a copy of the question:

https://community.nxp.com/thread/470763 

0 Kudos