Changing the MDC speed in P2041

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing the MDC speed in P2041

1,067件の閲覧回数
sameerarvikar
Contributor III

I probed mdc ,and got to know that

when uboot is running mdc speed is 4.7 MHz

where as linux boots up speed reduces to 1.8 MHz

How to increase the MDC speed

cannot find any register to change the mdc clock frequency  in P2041 RM

タグ(2)
0 件の賞賛
返信
1 返信

994件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

You can find the MDIO registers in QorIQ Data Path Acceleration Architecture (DPAA) Reference Manual. You can download it from the nxp site page

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-pla...

Please see MDIO Configuration and Status Register (MDIO_CFG_STAT). MDIO_CFG_STAT[MDIO_CLK_DIV] configures the MDIO clock frequency.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信