Can LS1046A and LS1026A share Same Openwrt source cord?

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Can LS1046A and LS1026A share Same Openwrt source cord?

301件の閲覧回数
ken_jung
Contributor I

Can LS1046A and LS1026A share Same Openwrt source cord?

0 件の賞賛
1 返信

189件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, both devices are based on the same silicon, the difference is only in number of cores (LS1026A has 2 cores instead of 4), so the software designed for LS1046A will work on LS1026A with very little or no modifications.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛