CPU1: failed to come online

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPU1: failed to come online

3,385 Views
brucezhao
Contributor I

Hello, 

      I have the same problem as the topic CPU1 failed to come online  , I do not find how that problem was solved.

      I use the SDK 2017-03 version. And NXP FAE told me that he do not know how to solve this.

     My cpu is ls1021a, 

     The board in question is costmized by us, took LS1021ATWR as refference.

     I have saved all the messages except emmc info coming out from u-boot and from the linux boot loader in the attached file.

    Thank you.

0 Kudos
Reply
7 Replies

2,012 Views
Pavel
NXP Employee
NXP Employee

Send information about your SDK. Is it SDK 2.0-1703?

See the following page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

Is there problem if this image is loaded to the TWR-LS1021a board?


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,012 Views
brucezhao
Contributor I

Yes, I followed the pdf QorIQ-SDK-2.0-1703-IC-Rev0.pdf. But it not list the git command to download the latest code. I google it and I found git pull origin jethro-sdk-v2.0-ga-17.03 to download linux kernel. Can you provide u-boot git command?

I replace with the latest kernel, still Cpu1 failed to come online.

0 Kudos
Reply

2,012 Views
brucezhao
Contributor I

I have solved this problem, thank you very much.

0 Kudos
Reply

2,012 Views
AshishYadav
Contributor I

Hi,

How you resolve this issue.

Thanks 

0 Kudos
Reply

2,012 Views
Pavel
NXP Employee
NXP Employee

Se
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,012 Views
brucezhao
Contributor I

Hi,

    I test ram under u-boot, and there is no errors.

=> mtest 0x80000000 0x9fffffff 0x5a5a5a5a 2
Testing 80000000 ... 9fffffff:
Pattern A5A5A5A5 Writing... Reading...Tested 2 iteration(s) with 0 errors.

 I also check the device tree, I found I modified nothing about CPU, just the same as nxp provided.

dts in u-boot:

cpus {
#address-cells = <1>;
#size-cells = <0>;

cpu@f00 {
compatible = "arm,cortex-a7";
device_type = "cpu";
reg = <0xf00>;
clocks = <&cluster1_clk>;
};

cpu@f01 {
compatible = "arm,cortex-a7";
device_type = "cpu";
reg = <0xf01>;
clocks = <&cluster1_clk>;
};
};

dts in kernel:

cpus {
#address-cells = <1>;
#size-cells = <0>;

cpu0: cpu@f00 {
compatible = "arm,cortex-a7";
device_type = "cpu";
reg = <0xf00>;
clocks = <&cluster1_clk>;
#cooling-cells = <2>;
};

cpu1: cpu@f01 {
compatible = "arm,cortex-a7";
device_type = "cpu";
reg = <0xf01>;
clocks = <&cluster1_clk>;
};
};

0 Kudos
Reply

2,011 Views
Pavel
NXP Employee
NXP Employee

Check CPU configuration in your device tree file.

Test your board using a DDR test. For example test DDR under u-boot.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply