Booting LS1021ATSN-PA with Pre-build Images

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting LS1021ATSN-PA with Pre-build Images

508 Views
jannisjoachimha
Contributor I

Dear NPX Community,
our Team recently owned a LS1021ATSN-PA. We tried to boot the Bridge by using the Images from the argonboard-webpage and following the steps of the .txt which comes with the files. Everything worked fine but the Bridge won’t start in U-Boot and copying the files.  We tried it with the 8 GB sd card which came with the bundle and a 32 GB card. The result was the same. The Serial connection works but the Terminal keeps blank.

Thanks in advance. Jannis

0 Kudos
1 Reply

338 Views
Pavel
NXP Employee
NXP Employee

The LS1021ATSN board uses CMSIS-DAP interface for serial communication.

Windows PC driver for serial communication is available on the following page:

https://developer.mbed.org/handbook/Windows-serial-configuration

 

Is this drive installed on your PC?

See also the following page:

https://community.nxp.com/thread/442615


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos