Boot from SPI NOR flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot from SPI NOR flash?

Jump to solution
1,548 Views
trondwang
Contributor I

Hi NXP,

the reference board LS1043ARDB-PA/PB has a SPI NOR flash (U32). Is it possible to boot from a SPI NOR flash by a RCW setting?

regards

Trond Inge

Tags (1)
0 Kudos
Reply
1 Solution
1,412 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, booting from this device is supported. Please refer to deployment guide in Linux SDK documentation precise instruction.

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-3E22804D-DD1E-43D7-AF28-8...


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,413 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, booting from this device is supported. Please refer to deployment guide in Linux SDK documentation precise instruction.

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-3E22804D-DD1E-43D7-AF28-8...


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply