Binary for AQR107 flash in LS1046ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Binary for AQR107 flash in LS1046ARDB

Jump to solution
3,808 Views
ken_jung
Contributor I

I am trying to get the  binary file for AQR107 flash in LS1046ARDB.

I asked Aquatina for the binary, then they asked to fill in the excel sheet attached.

Can I use the default setting int the excel sheet or do I  have to change something to match with LS1046ARDB?   

Can NXP provide binary file which is used for AQR107 flash in LS1046ARDB?

0 Kudos
1 Solution
3,350 Views
ufedor
NXP Employee
NXP Employee

Please refer to the attached files from the factory.

View solution in original post

0 Kudos
11 Replies
3,239 Views
changjake
Contributor II

Hi ufdor,

 

I tried, but got follow result of haning.

==================

=> tftp 82000000 aq_programming.bin
Using FM1@DTSEC4 device
TFTP from server 192.168.1.10; our IP address is 192.168.1.100
Filename 'aq_programming.bin'.
Load address: 0x82000000
Loading: #############
35.2 KiB/s
done
Bytes transferred = 180944 (2c2d0 hex)
=> tftp 84000000 AQR-G2_v3.3.D-AQR_Freescale_AQR107_ID16066_VER554.cld
Using FM1@DTSEC4 device
TFTP from server 192.168.1.10; our IP address is 192.168.1.100
Filename 'AQR-G2_v3.3.D-AQR_Freescale_AQR107_ID16066_VER554.cld'.
Load address: 0x84000000
Loading: #####################
9.3 MiB/s
done
Bytes transferred = 303106 (4a002 hex)
=> go 0x82000000 FM1@TGEC1 0x84000000 0x4a002
## Starting application at 0x82000000 ...
"Synchronous Abort" handler, esr 0x8600000e
elr: ffffffff443d8000 lr : ffffffffc63d805c (reloc)
elr: 0000000000000000 lr : 000000008200005c
x0 : 00000000fbc28fd0 x1 : 000000008202c2d0
x2 : 00000000fbc29048 x3 : 0000000000000001
x4 : 00000000ffffffff x5 : 00000000fbc20f28
x6 : 0000000000000030 x7 : 000000000000000f
x8 : 00000000fbc21398 x9 : 0000000000000000
x10: 00000000ffffffd0 x11: 0000000000000010
x12: 0000000000000004 x13: 0000000000000200
x14: 0000000000000002 x15: 0000000000000001
x16: 0000000082000000 x17: 00000000fbdb4ad1
x18: 00000000fbc23d70 x19: 00000000fbc29048
x20: 0000000000000004 x21: 0000000000000005
x22: 00000000fbc29040 x23: 00000000fbdd57b8
x24: 0000000000000005 x25: 0000000000000000
x26: 0000000000000000 x27: 0000000000000000
x28: 00000000fbc29080 x29: 00000000fbc21390

Resetting CPU ...

resetting ...

===================

 

Maybe, I think that flash of AQR107 is not clean.

Is there anyway to clean previous firmware?

 

T.I.A.

0 Kudos
3,350 Views
ken_jung
Contributor I

"after SMT is done" means after parts are mounted  on the PCB board and soldered in refolw in the SMT(SMD) factory.  

And what I want to do is to write indetendently flash memory of AQR107 using ROM writer before SMT process, so that programing process can be skiped after SMT process.     

0 Kudos
3,350 Views
ken_jung
Contributor I

Ok

Thanks

0 Kudos
3,350 Views
ufedor
NXP Employee
NXP Employee

Sorry, there is no such solution from NXP.

0 Kudos
3,350 Views
ken_jung
Contributor I

The text file explains how to program firmware of AQR107 after SMT is done.

And cld file is firmware to be written to flash memory of AQR107.

Then, can I write cld file directly to flash memory of AQR107 using ROM writer before SMT?

0 Kudos
3,350 Views
ufedor
NXP Employee
NXP Employee

> after SMT is done

What do you mean?

0 Kudos
3,350 Views
ken_jung
Contributor I

I am asking this question, because I am designing a router based on LS1046ARDB. And I need to write the SPI flash memory which is connected to AQR107 before  SMT of PCB. I don't have any intension to change any configuration of the interface between LS1046A and AQR107 from LS1046ARDB.

In the release note(.pdf), above comment " Remove The Following Customer Notes Section" appears.

 I am asking if I need to do something to the cld file about this comment, and If the cld file can be written just by defining as a binary file in the memory writing tool or need any compiling before writing. 

0 Kudos
3,351 Views
ufedor
NXP Employee
NXP Employee

Please refer to the attached files from the factory.

0 Kudos
3,350 Views
ken_jung
Contributor I
  1. Does the cld file require any modification to follow below note in pdf file

***Start: Remove The Following Customer Notes Section**** Product branch top-level provisioning: SMBus Address = 0 Enables user control of the LED outputs Enables LED0 Enables LED1 Disables LED2 LED0, LED1, LED2 OFF Disable 10GBASE-T Advertisement Disable 5GBASE-T and 5G NBASE-T Advertisement Disable 2.5GBASE-T and 2.5G NBASE-T Advertisement Disable 1000BASE-T Advertisement Disable 100BASE-TX FD/HD and Pause/AsymPause Advertisement DTE Detection Disabled ANEG Timeout set to = 6 seconds Counter Read Order = MSW First ***End: Remove The Following Customer Notes Section****


  1. Usually binary file has bin file extender.

    Does the cld file requires compiling to write the flash of AQR107 or can it be written to the flash directly as a binary?  

0 Kudos
3,350 Views
ufedor
NXP Employee
NXP Employee

Normally it is not supposed that customers will program the AQR107 firmware because the RDB board is properly programmed at the factory.

0 Kudos
3,350 Views
ufedor
NXP Employee
NXP Employee

Please find the binary image attached.

0 Kudos