Hi experts,
I did some audio testing on ls1028ardb based on the section 4.1.14.3 Synchronous audio interface (SAI) from "Layerscape LS1028A BSP v0.2.pdf", I did set the sw5(8) on, and BRDCFG3[2] = 1, then run the default Image from emmc, it seems still failure with the followings:
root@ls1028a:/# uname -a
Linux ls1028a 4.14.47-51091-g985a1f51c31c #2 SMP PREEMPT Wed Dec 19 11:41:09 IST 2018 aarch64 GNU/Linux
root@ls1028a:/# aplay ./usr/share/sounds/alsa/Rear_Center.wav
Playing WAVE './usr/share/sounds/alsa/Rear_Center.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Mono
aplay: pcm_write:1947: write error: Input/output error
root@ls1028a:/#
root@ls1028a:/#
root@ls1028a:/# aplay ./usr/share/sounds/alsa/Rear_Center.wav
Playing WAVE './usr/share/sounds/alsa/Rear_Center.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Mono
aplay: pcm_write:1947: write error: Input/output error
root@ls1028a:/#
root@ls1028a:/# aplay ./run/media/mmcblk0p3/mnt/44k-16b.wav
Playing WAVE './run/media/mmcblk0p3/mnt/44k-16b.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
aplay: pcm_write:1947: write error: Input/output error
root@ls1028a:/# aplay -f S16_LE -r 44100 -t wav -c 2 ./run/media/mmcblk0p3/mnt/44k-16b.wav
Playing WAVE './run/media/mmcblk0p3/mnt/44k-16b.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
aplay: pcm_write:1947: write error: Input/output error
Any comments are welcome
Cheers,
Zumeng
已解决! 转到解答。
Please refer to the following.
=> tftp a0000000 rcw_1300_audio.bin
=> sf probe 0:0
=> sf erase 0 +$filesize && sf write 0xa0000000 0 $filesize
=> reset
Thanks,
Yiping
Hello zumeng chen,
I confirmed with Linux SDK testing team, they have verified SAI audio driver on LS1028ARDB following BSP 0.2 user manual without any problem.
Please use rcw_1300_audio.bin for audio function(EC1_SAI4_5_PMUX = 2), please refer to the attachment.
In Linux please type the following command "zcat /proc/config.gz>config.txt", and check whether the following options are enabled in config.txt
CONFIG_I2C_IMX=y
CONFIG_SOUND=y
CONFIG_SND=y
CONFIG_SND_PCM_OSS=y
CONFIG_SND_PCM_OSS_PLUGINS=y
CONFIG_SND_SUPPORT_OLD_API=y
CONFIG_SND_SOC_FSL_SAI=y
CONFIG_SND_SOC_GENERIC_DMAENGINE_PCM=y
CONFIG_SND_SIMPLE_CARD=y
CONFIG_SND_SOC_SGTL5000=y
CONFIG_FSL_EMDA=y
On ls1028ardb board, please do the following operations.
a. Set the switch SW5[8] = ON.
b. To configure BRDCFG3[2] = 1, run the following command at U-Boot prompt.
i2c mw 0x66 0x53 0x4
c. The lineout interface is J34.
If your problem remains, please capture the console log including u-boot, Linux Kernel booting up and all your operations under Linux.
Thanks,
Yiping
En, I guess I might forget to update rcw, I'll take a look tomorrow, then feed back to you, thanks~
BTW, could you please give me a link to a documentation file how to update RCW if convenience.
Cheers,
Zumeng