Anyone using Lauderbach JTAG to LS1043ARDB development board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anyone using Lauderbach JTAG to LS1043ARDB development board.

1,422 Views
joe_freeman
Contributor I

Does anyone have the CMSIS-DAP configuration parameter for the Lauderbach JTAG Debugger?

And no I do not want to buy Codewarrior for ~$8,000 and a CodeWarrior USB TAP for ~$600.

Is there anyway to disable the Kinetis K22 MCU. And use the JTAG interface?

Thanks,

0 Kudos
Reply
1 Reply

1,353 Views
alexander_yakov
NXP Employee
NXP Employee

Kinetis K22 is used to implement CMSIS-DAP interface, which is an interface between USB and processor debug port. Yes, there is a way to disable it and use JTAG pins to connect external debug probe, for example CodeWarrior TAP. To disable CMSIS-DAP please switch SW3[6]. 

CodeWarrior IDE is our integrated development environment, it consists of a number of tools - compiller, linker, debugger, flash prorrammer, hardware diagnostics tools, configuration tool, DDR memory validation tool and etc. 30-days evaluation version is available for free, you can test all functions before purchase. Annual price starts from $2999 (for developer suite).

CodeWarrior TAP is debug probe for CodeWarrior software, this is relatively complex device with its own processor and operating system inside, but not just a simple "adapter". If the price of this device is not acceptable, than there are several other options - you can use CMSIS-DAP for example.   

Lauterbach software is supported by Lauterbach company, please address Lauterbach-related questions to this company directly. Here is a direct link to support page at their public site:

https://www.lauterbach.com/tsupport.html

0 Kudos
Reply