Activate X-server or Wayland on T1042D4RDB-64b ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activate X-server or Wayland on T1042D4RDB-64b ?

ソリューションへジャンプ
768件の閲覧回数
yusufalti333
Contributor IV

Hello,

What is the procedure to activate X-server or Wayland on T1042D4RDB-64B. I see IMX BSP's are having these. Can we use similar recipes for T1042D4RDB-64B. I am trying to take a VGA output from External GPU ( Connected via PCIe ).

And also what is the procedure to active video output from U-boot for external GPU's ?

Thanks.

0 件の賞賛
1 解決策
699件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Yusuf Altıparmak,

Please execute command "bitbake core-image-weston" to generate image with X-server and Wayland enabled.

Under u-boot

For SHARP LCD panel through LVDS interface:
=>setenv video-mode ‘fslfb:800x600-32@60,monitor=lvds’
For monitor through DVI interface:
=>setenv video-mode ‘fslfb:1024x768-32@60,monitor=dvi’

Thanks,

Yiping

元の投稿で解決策を見る

0 件の賞賛
1 返信
700件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Yusuf Altıparmak,

Please execute command "bitbake core-image-weston" to generate image with X-server and Wayland enabled.

Under u-boot

For SHARP LCD panel through LVDS interface:
=>setenv video-mode ‘fslfb:800x600-32@60,monitor=lvds’
For monitor through DVI interface:
=>setenv video-mode ‘fslfb:1024x768-32@60,monitor=dvi’

Thanks,

Yiping

0 件の賞賛