安装完sdk后能进行哪些开发

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

安装完sdk后能进行哪些开发

949 Views
lingyunhui
Contributor I

安装完sdk后能进行哪些开发

0 Kudos
4 Replies

880 Views
lunminliang
NXP Employee
NXP Employee

Hi,

你需要做啥开发呢?给出你的具体需求也许能获得更进一步的帮助。

Regards

Lunmin

0 Kudos

880 Views
lingyunhui
Contributor I

修改linux kernel,c语言交叉编译环境

0 Kudos

880 Views
lunminliang
NXP Employee
NXP Employee

Hi,

你好。

可以的。步骤如下:

1. Modify kernel source code

a. $ bitbake -c cleansstate virtual/kernel

b. $ bitbake -c patch virtual/kernel

c. $ cd <S> and change the source code

                                    NOTE

Use bitbake -e <package-name> | grep ^S= get the value of

<S>.

2. Change the kernel defconfig

a. $ update KERNEL_DEFCONFIG variable in meta-fsl-ppc/conf/machine/<machine>.conf

3. Change dts

a. $ update KERNEL_DEVICETREE variable in meta-fsl-ppc/conf/machine/<machine>.conf

4. Do menuconfig

a. $ bitbake -c menuconfig virtual/kernel

5. Rebuild Kernel image

a. $ cd build_<machine>_release

b. $ bitbake -c compile -f virtual/kernel

c. $ bitbake virtual/kernel

这个步骤可以在飞思卡尔官网的在线信息中心中找到:

Freescale Technical Information Center


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

880 Views
lingyunhui
Contributor I

那如何进行gcc交叉编译

0 Kudos