The system will print “**printk messages dropped” continuously when reboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The system will print “**printk messages dropped” continuously when reboot

8,499 Views
zhimingqiu
Contributor I

my cpu is B4860 and I use the the sdk-v2.0-1703; my problem is : When the system restarts,Occasionally, The system will print “**printk messages dropped” continuously at the following locations:

[11:15:56]U-Boot 2016.09-svn251626 (V3.0.0-5 Nov 13 2018 - 11:37:03)
[11:15:56]
[11:15:56]CPU0: B4860E, Version: 2.2, (0x86880022)
[11:15:56]Core: e6500, Version: 2.0, (0x80400120)
[11:15:56]Clock Configuration:
[11:15:56] CPU0:1600 MHz, CPU1:1600 MHz, CPU2:1600 MHz, CPU3:1600 MHz,
[11:15:56] DSP CPU0:1200 MHz, DSP CPU1:1200 MHz, DSP CPU2:1200 MHz, DSP CPU3:1200 MHz,
[11:15:56] DSP CPU4:1200 MHz, DSP CPU5:1200 MHz,
[11:15:56] CCB:666.667 MHz,
[11:15:56] DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:333.333 MHz
[11:15:56] CPRI:600 MHz
[11:15:56] MAPLE:600 MHz, MAPLE-ULB:800 MHz, MAPLE-eTVPE:1000 MHz
[11:15:56] FMAN1: 666.667 MHz
[11:15:56] QMAN: 333.333 MHz
[11:15:56]L1: D-cache 32 KiB enabled
[11:15:56] I-cache 32 KiB enabled
[11:15:56]Reset Configuration Word (RCW):
[11:15:56] 00000000: 14000c18 0f001218 00000000 00000000
[11:15:56] 00000010: 5a040000 20900000 ec025000 a9000000
[11:15:56] 00000020: 00000000 00000001 00000000 100071fc
[11:15:56] 00000030: 00000100 04000020 00000000 00000011
[11:15:56]RCW src = 0x049 (I2C1 extended addressing)
[11:15:57]RCW GPINFO = 00000001, CRC = 0x48cb7a27
[11:15:57]Board: B4860, boot from NOR FLASH bank 1
[11:15:57]SERDES Reference Clocks: SD1_CLK1=0, SD1_CLK2=122.88 SD2_CLK1=125, SD2_CLK2=0
[11:15:57]Serdes1 PLL1 is powered down.
[11:15:57]Serdes2 PLL2 is powered down.
[11:15:57]Reset Request Mask Register: 0x00004000
[11:15:57]Reset Request Status Register: 0x00100000
[11:15:57]I2C: ready
[11:15:57]SPI: ready
[11:15:57]DRAM: Initializing....using SPD
[11:15:57]Detected UDIMM RAW timing DDR
[11:15:57]Detected UDIMM RAW timing DDR
[11:15:58]3 GiB left unmapped
[11:15:58]5 GiB (DDR3, 64-bit, CL=11, ECC on)
[11:15:58]VID: DCFG_CCSR_FUSESR=0x20000000. DA_V=0x10, DA_ALT_V=0x00. VID=0x10, vdd=1.0000 V
[11:15:58]VID: target vid = 1000.0 mV
[11:15:58]VID: Core voltage is currently at 0.9935 V from sensor (setting 1.0000 V)
[11:15:58]VID: Core voltage is equal to the setting. Nothing is changed.
[11:15:58]Flash: 128 MiB
[11:15:58]L2: 2 MiB enabled
[11:15:58]Corenet Platform Cache: 512 KiB enabled
[11:15:58]Using SERDES1 Protocol: 45 (0x2d)
[11:15:58]Using SERDES2 Protocol: 4 (0x4)
[11:15:58]SEC0: RNG instantiated
[11:15:58]NAND: 1024 MiB
[11:15:58]In: serial
[11:15:58]Out: serial
[11:15:58]Err: serial
[11:15:58]do_flash_bank_select() cpld reg 0x32=0x1 0x33=0x0 0x34=0x66
[11:15:58]Net: Initializing Fman
[11:15:58]Fman1: Uploading microcode version 106.4.18
[11:15:58]FM1@DTSEC1 [PRIME], FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4
[11:15:59]WARNING: adjusting available memory to 30000000
[11:15:59]## Booting kernel from Legacy Image at ec100000 ...
[11:15:59] Image Name: Linux-4.1.35-rt41
[11:15:59] Image Type: PowerPC Linux Kernel Image (gzip compressed)
[11:15:59] Data Size: 5783939 Bytes = 5.5 MiB
[11:15:59] Load Address: 00000000
[11:15:59] Entry Point: 00000000
[11:16:01] Verifying Checksum ... OK
[11:16:01]## Loading init Ramdisk from Legacy Image at ecb00000 ...
[11:16:01] Image Name: Ram disk 
[11:16:01] Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
[11:16:01] Data Size: 34130794 Bytes = 32.5 MiB
[11:16:01] Load Address: 00000000
[11:16:01] Entry Point: 00000000
[11:16:08] Verifying Checksum ... OK
[11:16:08]## Flattened Device Tree blob at ec0e0000
[11:16:08] Booting using the fdt blob at 0xec0e0000
[11:16:10] Uncompressing Kernel Image ... OK
[11:16:10] reserving fdt memory region: addr=fec00000 size=40000
[11:16:10] reserving fdt memory region: addr=fffe0000 size=20000
[11:16:17] Loading Ramdisk to 01f73000, end 03fffb6a ... OK
[11:16:17] Loading Device Tree to 01f56000, end 01f72c9c ... OK
[11:16:18]WARNING Could not get liodn of node /pcie@ffe200000: FDT_ERR_NOTFOUND
[11:16:18][ 0.000000] Using fsl_fm_max_frm=9600 from bootargs
[11:16:18][ 0.000000] uspdaa_mem argument is depracated
[11:16:18][ 0.000000] Reserved memory: initialized node bman-fbpr, compatible id fsl,bman-fbpr
[11:16:18][ 0.000000] Reserved memory: initialized node qman-fqd, compatible id fsl,qman-fqd
[11:16:18][ 0.000000] Reserved memory: initialized node qman-pfdr, compatible id fsl,qman-pfdr
[11:16:18][ 0.000000] Reserved memory: initialized node usdpaa_mem, compatible id fsl,usdpaa-mem
[11:16:18][ 0.000000] Using CoreNet Generic machine description
[11:16:18][ 0.000000] MMU: Supported page sizes
[11:16:18][ 0.000000] 4 KB as direct
[11:16:18][ 0.000000] 2048 KB as direct & indirect
[11:16:18][ 0.000000] 4096 KB as direct
[11:16:18][ 0.000000] 16384 KB as direct
[11:16:18][ 0.000000] 65536 KB as direct
[11:16:18][ 0.000000] 262144 KB as direct
[11:16:18][ 0.000000] 1048576 KB as direct
[11:16:18][ 0.000000] MMU: Book3E HW tablewalk enabled
[11:16:18][ 0.000000] Found initrd at 0xc000000001f73000:0xc000000003fffb6a
[11:16:18] <- setup_system()
[11:16:18][ 0.000000] bootconsole [udbg0] enabled
[11:16:18][ 0.000000] CPU maps initialized for 2 threads per core
[11:16:18][ 0.000000] Starting Linux PPC64 #18 SMP PREEMPT RT Thu Sep 26 16:34:08 CST 2019
[11:16:18][ 0.000000] -----------------------------------------------------
[11:16:18][ 0.000000] ppc64_pft_size = 0x0
[11:16:18][ 0.000000] phys_mem_size = 0x100000000
[11:16:18][ 0.000000] dcache_line_size = 0x40
[11:16:18][ 0.000000] icache_line_size = 0x40
[11:16:18][ 0.000000] cpu_features = 0x00180480581802c8
[11:16:18][ 0.000000] possible = 0x00180480581802c8
[11:16:18][ 0.000000] always = 0x00180400581802c0
[11:16:18][ 0.000000] cpu_user_features = 0xdc008000 0x08000000
[11:16:18][ 0.000000] mmu_features = 0x000a0010
[11:16:18][ 0.000000] firmware_features = 0x0000000000000000
[11:16:18][ 0.000000] -----------------------------------------------------
[11:16:18][ 0.000000] Initializing cgroup subsys cpuset
[11:16:18][ 0.000000] Initializing cgroup subsys cpu
[11:16:18][ 0.000000] Initializing cgroup subsys cpuacct
[11:16:18][ 0.000000] Linux version 4.1.35-rt41 + (root@nansn) (gcc version 4.8.1 (GCC) ) #18 SMP PREEMPT RT Thu Sep 26 16:34:08 CST 2019
[11:16:18][ 0.000000] (kernel version: V1.1.0-1)
[11:16:18][ 0.000000] CoreNet Generic board
[11:16:18][ 0.000000] Zone ranges:
[11:16:18][ 0.000000] DMA [mem 0x0000000000000000-0x00000000ffffffff]
[11:16:18][ 0.000000] DMA32 empty
[11:16:18][ 0.000000] Normal empty
[11:16:18][ 0.000000] Movable zone start for each node
[11:16:18][ 0.000000] Early memory node ranges
[11:16:18][ 0.000000] node 0: [mem 0x0000000000000000-0x00000000ffffffff]
[11:16:18][ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x00000000ffffffff]
[11:16:18][ 0.000000] MMU: Allocated 2112 bytes of context maps for 255 contexts
[11:16:18][ 0.000000] PERCPU: Embedded 158 pages/cpu @c0000000fe400000 s607744 r0 d39424 u1048576
[11:16:18][ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1032192
[11:16:18][ 0.000000] Kernel command line: root=/dev/ram rw console=ttyS1,115200 fsl_fm_max_frm=9600 default_hugepagesz=256m hugepagesz=256m hugepages=1 usdpaa_mem=512M hostname=b4860_bld_bbu tty_magic
[11:16:18][ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[11:16:18][ 0.000000] Dentry cache hash table entries: 524288 (order: 11, 8388608 bytes)
[11:16:18][ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[11:16:18][ 0.000000] Sorting __ex_table...
[11:16:18][ 0.000000] Memory: 3150960K/4194304K available (9960K kernel code, 1684K rwdata, 3168K rodata, 1236K init, 1549K bss, 1043344K reserved, 0K cma-reserved)
[11:16:18][ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=8, Nodes=1
[11:16:18][ 0.000000] Preemptible hierarchical RCU implementation.
[11:16:18][ 0.000000] Additional per-CPU info printed with stalls.
[11:16:18][ 0.000000] RCU kthread priority: 1.
[11:16:18][ 0.000000] NR_IRQS:512 nr_irqs:512 16
[11:16:18][ 0.000000] mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs
[11:16:18][ 0.000000] mpic: ISU size: 512, shift: 9, mask: 1ff
[11:16:18][ 0.000000] mpic: Initializing for 512 sources
[11:16:18][ 0.000004] clocksource timebase: mask: 0xffffffffffffffff max_cycles: 0x99c0f5e04, max_idle_ns: 440795204113 ns
[11:16:18][ 0.000008] clocksource: timebase mult[18000006] shift[24] registered
[11:16:18][ 0.001807] Console: colour dummy device 80x25
[11:16:18][ 0.279849] pid_max: default: 32768 minimum: 301
[11:16:18][ 0.279916] Security Framework initialized
[11:16:18][ 0.280012] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[11:16:18][ 0.280018] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[11:16:18][ 0.280598] Initializing cgroup subsys blkio
[11:16:18][ 0.280607] Initializing cgroup subsys memory
[11:16:18][ 0.280637] Initializing cgroup subsys devices
[11:16:18][ 0.280645] Initializing cgroup subsys freezer
[11:16:18][ 0.280653] Initializing cgroup subsys net_cls
[11:16:18][ 0.280660] Initializing cgroup subsys debug
[11:16:18][ 0.280679] ftrace: allocating 23956 entries in 141 pages
[11:16:19][ 0.300331] e6500 family performance monitor hardware support registered
[11:16:19][ 0.440627] Brought up 8 CPUs
[11:16:19][ 0.444186] devtmpfs: initialized
[11:16:19][ 0.461560] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[11:16:19][ 0.472322] NET: Registered protocol family 16
[11:16:19][ 0.477270] Bman ver:0a02,02,01
[11:16:19][ 0.580656] qman-fqd addr 0x00000000ff000000 size 0x800000
[11:16:19][ 0.586051] qman-pfdr addr 0x00000000fa000000 size 0x2000000
[11:16:19][ 0.591702] Qman ver:0a01,03,01,01
[11:16:19][ 0.685960] pps_core: LinuxPPS API ver. 1 registered
[11:16:19][ 0.690839] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[11:16:19][ 0.699979] PTP clock support registered
[11:16:19][ 0.703912] EDAC MC: Ver: 3.0.0
[11:16:19][ 0.707326] bman-fbpr addr 0x00000000fd000000 size 0x1000000
[11:16:19][ 0.713066] Bman err interrupt handler present
[11:16:19][ 0.719000] Bman portal initialised, cpu 0
[11:16:19][ 0.723168] Bman portal initialised, cpu 1
[11:16:19][ 0.727341] Bman portal initialised, cpu 2
[11:16:19][ 0.731520] Bman portal initialised, cpu 3
[11:16:19][ 0.735688] Bman portal initialised, cpu 4
[11:16:19][ 0.739855] Bman portal initialised, cpu 5
[11:16:19][ 0.744030] Bman portal initialised, cpu 6
[11:16:19][ 0.748205] Bman portal initialised, cpu 7
[11:16:19][ 0.752209] Bman portals initialised
[11:16:19][ 0.756455] Qman err interrupt handler present
[11:16:19][ 0.761489] QMan: Allocated lookup table at 8000000000002000, entry count 131073
[11:16:19][ 0.770569] Qman portal initialised, cpu 0
[11:16:19][ 0.774768] Qman portal initialised, cpu 1
[11:16:19][ 0.778975] Qman portal initialised, cpu 2
[11:16:19][ 0.783180] Qman portal initialised, cpu 3
[11:16:19][ 0.787378] Qman portal initialised, cpu 4
[11:16:19][ 0.791582] Qman portal initialised, cpu 5
[11:16:19][ 0.795800] Qman portal initialised, cpu 6
[11:16:19][ 0.799999] Qman portal initialised, cpu 7
[11:16:19][ 0.804003] Qman portals initialised
[11:16:19][ 0.807727] Bman: BPID allocator includes range 32:32
[11:16:19][ 0.812797] Qman: FQID allocator includes range 256:512
[11:16:19][ 0.817934] Qman: FQID allocator includes range 32768:32768
[11:16:19][ 0.823592] Qman: CGRID allocator includes range 0:256
[11:16:19][ 0.828864] Qman: pool channel allocator includes range 1025:15
[11:16:19][ 0.834885] USDPAA region at c0000000:20000000(c0000:20000), 1 TLB1 entries)
[11:16:19][ 0.841890] fsl-ifc ffe124000.localbus: Freescale Integrated Flash Controller
[11:16:19][ 0.848981] fsl-ifc ffe124000.localbus: IFC version 1.1, 8 banks
[11:16:19][ 0.856452] Switched to clocksource timebase
[11:16:19][ 0.938638] NET: Registered protocol family 2
[11:16:19][ 0.943548] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[11:16:19][ 0.950995] TCP bind hash table entries: 32768 (order: 8, 1835008 bytes)
[11:16:19][ 0.958522] TCP: Hash tables configured (established 32768 bind 32768)
[11:16:19][ 0.965062] UDP hash table entries: 2048 (order: 6, 262144 bytes)
[11:16:19][ 0.971211] UDP-Lite hash table entries: 2048 (order: 6, 262144 bytes)
[11:16:19][ 0.978037] NET: Registered protocol family 1
[11:16:19][ 0.982635] RPC: Registered named UNIX socket transport module.
[11:16:19][ 0.988465] RPC: Registered udp transport module.
[11:16:19][ 0.993157] RPC: Registered tcp transport module.
[11:16:19][ 0.997848] RPC: Registered tcp NFSv4.1 backchannel transport module.
[11:16:19][ 1.004580] Trying to unpack rootfs image as initramfs...
[11:16:19][ 1.010295] rootfs image is not initramfs (no cpio magic); looks like an initrd
[11:16:19][ 1.165289] Freeing initrd memory: 33328K (c000000001f73000 - c000000003fff000)
[11:16:19][ 1.173839] cryptomgr_test (107) used greatest stack depth: 13088 bytes left
[11:16:19][ 1.177520] futex hash table entries: 2048 (order: 6, 262144 bytes)
[11:16:19][ 1.188074] HugeTLB registered 256 MB page size, pre-allocated 1 pages
[11:16:19][ 1.194515] HugeTLB registered 4 MB page size, pre-allocated 0 pages
[11:16:19][ 1.200857] HugeTLB registered 16 MB page size, pre-allocated 0 pages
[11:16:19][ 1.207286] HugeTLB registered 64 MB page size, pre-allocated 0 pages
[11:16:19][ 1.213715] HugeTLB registered 1 GB page size, pre-allocated 0 pages
[11:16:19][ 1.232208] VFS: Disk quotas dquot_6.6.0
[11:16:19][ 1.236249] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[11:16:19][ 1.247192] NFS: Registering the id_resolver key type
[11:16:19][ 1.252179] Key type id_resolver registered
[11:16:19][ 1.256324] Key type id_legacy registered
[11:16:19][ 1.260363] jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
[11:16:19][ 1.267774] cryptomgr_test (112) used greatest stack depth: 12592 bytes left
[11:16:19][ 1.276525] cryptomgr_test (132) used greatest stack depth: 11424 bytes left
[11:16:19][ 1.278812] NET: Registered protocol family 38
[11:16:19][ 1.278825] Key type asymmetric registered
[11:16:19][ 1.278832] Asymmetric key parser 'x509' registered
[11:16:19][ 1.279100] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 251)
[11:16:19][ 1.279111] io scheduler noop registered
[11:16:19][ 1.279118] io scheduler deadline registered
[11:16:19][ 1.279328] io scheduler cfq registered (default)
[11:16:19][ 1.336866] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[11:16:19][ 1.345077] serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36, base_baud = 20833333) is a 16550A
[11:16:19]J+HH悙1.358260] serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36, base_baud = 20833333) is a 16550A
[11:16:19][ 1.366991] console [ttyS1] enabled
[11:16:19][ 1.366991] console [ttyS1] enabled
[11:16:20][ 1.373914] bootconsole [udbg0] disabled
[11:16:20][ 1.373914] bootconsole [udbg0] disabled
[11:16:20][ 1.382705] serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37, base_baud = 20833333) is a 16550A
[11:16:20][ 1.392480] serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37, base_baud = 20833333) is a 16550A
[11:16:20][ 1.409959] brd: module loaded
[11:16:20][ 1.418445] loop: module loaded
[11:16:20][ 1.426709] fe8000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000001 Chip ID 0x002801
[11:16:20][ 1.436803] Amd/Fujitsu Extended Query Table at 0x0040
[11:16:20][ 1.441948] Amd/Fujitsu Extended Query version 1.5.
[11:16:20][ 1.447001] number of CFI chips: 1
[11:16:20][ 1.451033] 18 ofpart partitions found on MTD device fe8000000.nor
[11:16:20][ 1.457212] Creating 18 MTD partitions on "fe8000000.nor":
[11:16:20][ 1.574676] nand: device found, Manufacturer ID: 0x01, Chip ID: 0xac
[11:16:20][ 1.581029] nand: AMD/Spansion S34MS04G1
[11:16:20][ 1.584950] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[11:16:20][ 1.593035] Bad block table found at page 262080, version 0x01
[11:16:20][ 1.599731] Bad block table found at page 262016, version 0x01
[11:16:20][ 1.606007] nand_read_bbt: bad block at 0x000011700000
[11:16:20][ 1.611573] 1 ofpart partitions found on MTD device fff800000.flash
[11:16:20][ 1.617839] Creating 1 MTD partitions on "fff800000.flash":
[11:16:20][ 1.623411] 0x000000000000-0x000020000000 : "user"
[11:16:20][ 1.629389] fsl,ifc-nand fff800000.nand: IFC NAND device at 0xfff800000, bank 1
[11:16:20][ 1.637595] nand: device found, Manufacturer ID: 0x01, Chip ID: 0xac
[11:16:20][ 1.643947] nand: AMD/Spansion S34MS04G1
[11:16:20][ 1.647868] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[11:16:20][ 1.655937] Bad block table found at page 262080, version 0x01
[11:16:20][ 1.662633] Bad block table found at page 262016, version 0x01
[11:16:20][ 1.668930] nand_read_bbt: bad block at 0x000004ec0000
[11:16:20][ 1.674068] nand_read_bbt: bad block at 0x000008bc0000
[11:16:20][ 1.679623] 1 ofpart partitions found on MTD device fff810000.flash
[11:16:20][ 1.685889] Creating 1 MTD partitions on "fff810000.flash":
[11:16:20][ 1.691461] 0x000000000000-0x000020000000 : "log"
[11:16:20][ 1.697327] fsl,ifc-nand fff810000.nand2: IFC NAND device at 0xfff810000, bank 2
[11:16:20][ 1.705605] fsl_espi ffe110000.spi: cs=0, init_csmode=0x100108
[11:16:20][ 1.711440] fsl_espi ffe110000.spi: cs=1, init_csmode=0x100108
[11:16:20][ 1.717792] fsl_espi ffe110000.spi: at 0x80000800809de000 (irq = 53)
[11:16:20][ 1.724872] libphy: Fixed MDIO Bus: probed
[11:16:20][ 1.730192] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.736218] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.741290] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.746362] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.751431] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.756536] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.761604] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.766673] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.771742] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.776814] libphy: Freescale XGMAC MDIO Bus: probed
[11:16:20][ 1.803052] Freescale FM module, FMD API version 21.1.0
[11:16:20][ 1.815964] Freescale FM Ports module
[11:16:20][ 1.819627] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[11:16:20][ 1.826059] fsl_mac ffe4e0000.ethernet: FMan MEMAC
[11:16:20][ 1.830855] fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:27:1d:00:00:0a
[11:16:20][ 1.838662] fsl_mac ffe4e2000.ethernet: FMan MEMAC
[11:16:20][ 1.843455] fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:27:1d:00:00:0b
[11:16:20][ 1.850997] fsl_mac ffe4e4000.ethernet: FMan MEMAC
[11:16:20][ 1.855791] fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:27:1d:28:e7:6b
[11:16:20][ 1.863579] fsl_mac ffe4e6000.ethernet: FMan MEMAC
[11:16:20][ 1.868373] fsl_mac ffe4e6000.ethernet: FMan MAC address: 00:27:1d:28:e7:6b
[11:16:20][ 1.875501] fsl_dpa: FSL DPAA Ethernet driver
[11:16:20][ 1.880478] fsl_mac ffe4e0000.ethernet: /soc@ffe000000/fman@400000/ethernet@e0000: ptp 1588 is initialized.
[11:16:20][ 1.907206] [dpaa_eth_priv_probe] , net_dev bpid = 32
[11:16:20][ 1.915023] fsl_dpa: fsl_dpa: Probed interface eth0
[11:16:20][ 1.920183] fsl_mac ffe4e2000.ethernet: /soc@ffe000000/fman@400000/ethernet@e2000: ptp 1588 is initialized.
[11:16:20][ 1.930297] [dpaa_eth_priv_probe] , net_dev bpid = 32
[11:16:20][ 1.937048] fsl_dpa: fsl_dpa: Probed interface eth1
[11:16:20][ 1.942140] fsl_mac ffe4e4000.ethernet: /soc@ffe000000/fman@400000/ethernet@e4000: ptp 1588 is initialized.
[11:16:20][ 1.952245] [dpaa_eth_priv_probe] , net_dev bpid = 32
[11:16:20][ 1.958948] fsl_dpa: fsl_dpa: Probed interface eth2
[11:16:20][ 1.964042] fsl_mac ffe4e6000.ethernet: /soc@ffe000000/fman@400000/ethernet@e6000: ptp 1588 is initialized.
[11:16:20][ 1.974145] [dpaa_eth_priv_probe] , net_dev bpid = 32
[11:16:20][ 1.980914] fsl_dpa: fsl_dpa: Probed interface eth3
[11:16:20][ 1.985891] cpu1/8: ! MAJOR FM-RTC Error [CPU01, ../drivers/net/ethernet/freescale/sdk_fman/Peripherals/FM/Rtc/fm_rtc.c:482 FM_RTC_SetAlarm]: Invalid Selection;
[11:16:20][ 2.000151] cpu1/8: Alarm time must be a multiple of RTC period - 8 nanoseconds[ 2.007461] cpu1/8:
[11:16:20][ 2.009729] FM_RTC_SetAlarm = 0x0004002b
[11:16:20][ 2.013653] cpu1/8: ! MAJOR FM-RTC Error [CPU01, ../drivers/net/ethernet/freescale/sdk_fman/Peripherals/FM/Rtc/fm_rtc.c:520 FM_RTC_SetPeriodicPulse]: Invalid Selection;
[11:16:20][ 2.028606] cpu1/8: Periodic pulse must be a multiple of RTC period - 8 nanoseconds[ 2.036263] cpu1/8:
[11:16:20][ 2.038531] FM_RTC_SetPeriodicPulse = 0x0004002b
[11:16:20][ 2.043485] pps pps0: new PPS source ptp0
[11:16:20][ 2.047497] fsl_advanced: FSL DPAA Advanced drivers:
[11:16:20][ 2.052488] fsl_proxy: FSL DPAA Proxy initialization driver
[11:16:20][ 2.058522] fsl_dpa_shared: FSL DPAA Shared Ethernet driver
[11:16:20][ 2.064535] fsl_dpa_macless: FSL DPAA MACless Ethernet driver
[11:16:20][ 2.070668] fsl_oh: FSL FMan Offline Parsing port driver
[11:16:20][ 2.076387] fsl_oh fsl,dpaa:dpa-fman0-oh@3: Found OH node handle compatible with fsl,dpa-oh
[11:16:20][ 2.084864] fsl_oh fsl,dpaa:dpa-fman0-oh@3: Allocating 0 ingress frame queues duples
[11:16:20][ 2.092744] fsl_oh fsl,dpaa:dpa-fman0-oh@3: IP Fragmentation enabled for OH port 2
[11:16:20][ 2.100565] fsl_oh fsl,dpaa:dpa-fman0-oh@3: OH port /soc@ffe000000/fman@400000/port@84000 enabled.
[11:16:20][ 2.109525] fsl_oh fsl,dpaa:dpa-fman0-oh@3: Default egress frame queue: 4055
[11:16:20][ 2.116574] fsl_oh fsl,dpaa:dpa-fman0-oh@3: Default error frame queue: 4054
[11:16:20][ 2.123535] fsl_oh fsl,dpaa:dpa-fman0-oh@3: Initialized queues:
[11:16:20][ 2.130261] fsl-of-dma ffe100300.dma: dma channel dma-uio0-0 initialized
[11:16:20][ 2.137262] fsl-of-dma ffe100300.dma: dma channel dma-uio0-1 initialized
[11:16:20][ 2.144272] fsl-of-dma ffe100300.dma: dma channel dma-uio0-2 initialized
[11:16:20][ 2.151280] fsl-of-dma ffe100300.dma: dma channel dma-uio0-3 initialized
[11:16:20][ 2.158287] fsl-of-dma ffe100300.dma: dma channel dma-uio0-4 initialized
[11:16:20][ 2.165291] fsl-of-dma ffe100300.dma: dma channel dma-uio0-5 initialized
[11:16:20][ 2.172303] fsl-of-dma ffe100300.dma: dma channel dma-uio0-6 initialized
[11:16:20][ 2.179313] fsl-of-dma ffe100300.dma: dma channel dma-uio0-7 initialized
[11:16:20][ 2.186353] fsl-of-dma ffe101300.dma: dma channel dma-uio1-0 initialized
[11:16:20][ 2.193360] fsl-of-dma ffe101300.dma: dma channel dma-uio1-1 initialized
[11:16:20][ 2.200370] fsl-of-dma ffe101300.dma: dma channel dma-uio1-2 initialized
[11:16:20][ 2.207388] fsl-of-dma ffe101300.dma: dma channel dma-uio1-3 initialized
[11:16:20][ 2.214402] fsl-of-dma ffe101300.dma: dma channel dma-uio1-4 initialized
[11:16:20][ 2.221418] fsl-of-dma ffe101300.dma: dma channel dma-uio1-5 initialized
[11:16:20][ 2.228472] fsl-of-dma ffe101300.dma: dma channel dma-uio1-6 initialized
[11:16:20][ 2.235475] fsl-of-dma ffe101300.dma: dma channel dma-uio1-7 initialized
[11:16:20][ 2.242308] i2c /dev entries driver
[11:16:20][ 2.246568] mpc-i2c ffe118000.i2c: timeout 1000000 us
[11:16:20][ 2.251914] at24 0-0050: 8192 byte 24c64 EEPROM, writable, 1 bytes/write
[11:16:20][ 2.258764] mpc-i2c ffe118100.i2c: timeout 1000000 us
[11:16:20][ 2.264254] mpc-i2c ffe119000.i2c: timeout 1000000 us
[11:16:20][ 2.269753] mpc-i2c ffe119100.i2c: timeout 1000000 us
[11:16:20][ 2.276053] lm75 2-0048: hwmon0: sensor 'lm75'
[11:16:21][ 2.381449] lm90 2-004c: device is in standby mode
[11:16:21][ 2.386590] lm90 2-004c: put device to run mode
[11:16:21][ 2.402117] zl6100 1-0019: Device ID ZLS1003-002FE07F
[11:16:21][ 2.511385] booke_wdt: powerpc book-e watchdog driver loaded
[11:16:21][ 2.517262] Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software
[11:16:21][ 2.525248] EDAC MC0: Giving out device to module MPC85xx_edac controller mpc85xx_mc_err: DEV mpc85xx_mc_err (INTERRUPT)
[11:16:21][ 2.536263] MPC85xx_edac acquired irq 475 for MC
[11:16:21][ 2.540878] MPC85xx_edac MC err registered
[11:16:21][ 2.545867] EDAC MC1: Giving out device to module MPC85xx_edac controller mpc85xx_mc_err: DEV mpc85xx_mc_err (INTERRUPT)
[11:16:21][ 2.556871] MPC85xx_edac acquired irq 476 for MC
[11:16:21][ 2.561486] MPC85xx_edac MC err registered
[11:16:21][ 2.568659] platform caam_qi: Linux CAAM Queue I/F driver initialised
[11:16:21][ 2.575104] caam ffe300000.crypto: Instantiated RNG4 SH1
[11:16:21][ 2.580571] caam ffe300000.crypto: device ID = 0x0a11020000000000 (Era 5)
[11:16:21][ 2.587359] caam ffe300000.crypto: job rings = 4, qi = 1
[11:16:21][ 2.598560] caam algorithms registered in /proc/crypto
[11:16:21][ 2.605998] platform caam_qi: algorithms registered in /proc/crypto
[11:16:21][ 2.614599] caam_jr ffe301000.jr: registering rng-caam
[11:16:21][ 2.620313] caam ffe300000.crypto: fsl,sec-v5.3 algorithms registered in /proc/crypto
[11:16:21][ 2.628527] fsl-of-rman ffe1e0000.rman: Of-device /soc@ffe000000/rman@1e0000 initialized
[11:16:21][ 2.636843] fsl-of-rman ffe1e0000.rman: RMan inbound block0 initialized.
[11:16:21][ 2.643713] fsl-of-rman ffe1e0000.rman: RMan inbound block1 initialized.
[11:16:21][ 2.650702] fsl-of-rman ffe1e0000.rman: RMan inbound block2 initialized.
[11:16:21][ 2.657567] fsl-of-rman ffe1e0000.rman: RMan inbound block3 initialized.
[11:16:21][ 2.666724] Freescale USDPAA process driver
[11:16:21][ 2.670999] Freescale USDPAA process IRQ driver
[11:16:21][ 2.676130] dce_sys_init done!
[11:16:21][ 2.679703] No fsl,dce node
[11:16:21][ 2.683018] Freescale pme2 db driver
[11:16:21][ 2.686590] PME2: fsl_pme2_db_init: not on ctrl-plane
[11:16:21][ 2.691644] Freescale pme2 scan driver
[11:16:21][ 2.695474] fsl-pme2-scan: device pme_scan registered
[11:16:21][ 2.700638] DPA Classifier Driver initialized.
[11:16:21][ 2.705183] DPA IPSec Driver initialized.
[11:16:21][ 2.709299] DPA Stats Driver initialized.
[11:16:21][ 2.713347] u32 classifier
[11:16:21][ 2.716048] Actions configured
[11:16:21][ 2.719463] Netfilter messages via NETLINK v0.30.
[11:16:21][ 2.724208] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[11:16:21][ 2.730749] nf_tables: (c) 2007-2009 Patrick McHardy <kaber@trash.net>
[11:16:21][ 2.737652] ip_tables: (C) 2000-2006 Netfilter Core Team
[11:16:21][ 2.743057] ipt_CLUSTERIP: ClusterIP Version 0.8 loaded successfully
[11:16:21][ 2.749454] Initializing XFRM netlink socket
[11:16:21][ 2.754577] NET: Registered protocol family 10
[11:16:21][ 2.759979] sit: IPv6 over IPv4 tunneling driver
[11:16:21][ 2.765120] NET: Registered protocol family 17
[11:16:21][ 2.769584] NET: Registered protocol family 15
[11:16:21][ 2.774085] 8021q: 802.1Q VLAN Support v1.8
[11:16:21][ 2.778324] sctp: Hash tables configured (established 73 bind 64/73)
[11:16:21][ 2.785147] Key type dns_resolver registered
[11:16:21][ 2.790807] console [netcon0] enabled
[11:16:21][ 2.794465] netconsole: network logging started
[11:16:21][ 2.798997] fsl_generic: FSL DPAA Generic Ethernet driver
[11:16:21][ 2.808574] RAMDISK: gzip image found at block 0
[11:16:24]** 267134 printk messages dropped ** [ 5.376041] [c0000000f2b73a80] [c0000000001e29a0] .__fput+0x1a0/0x290
[11:16:24]** 2313 printk messages dropped ** [ 5.385720] ---[ end trace 000000000000218d ]---
[11:16:24]** 1833 printk messages dropped ** [ 5.393380] ---[ end trace 00000000000021c8 ]---
[11:16:24]** 1839 printk messages dropped ** [ 5.401061] Call Trace:
[11:16:24]** 1324 printk messages dropped ** [ 5.406524] 81480010 38caffff 7cc65378 54c60ffe <0b060000> 394affff 2f8a0000 91480010
[11:16:24]** 2636 printk messages dropped ** [ 5.417492] NIP [c0000000000472f8] .unpin_current_cpu+0x48/0x90
[11:16:24]** 2155 printk messages dropped ** [ 5.426455] [c0000000f2b73520] [c00000000007eedc] .migrate_enable+0xec/0x270
[11:16:24]** 2432 printk messages dropped ** [ 5.436575] [c0000000f1143c60] [c000000000076a14] .smpboot_thread_fn+0x334/0x4b0
[11:16:24]** 2514 printk messages dropped ** [ 5.446983] Instruction dump:
[11:16:24]** 1436 printk messages dropped ** [ 5.452977] [c0000000f2b739c0] [c0000000001fd7c0] .dput+0x320/0x400
[11:16:24]** 2242 printk messages dropped ** [ 5.462284] NIP [c0000000000472f8] .unpin_current_cpu+0x48/0x90
[11:16:24]** 2164 printk messages dropped ** [ 5.471259] NIP [c0000000000472f8] .unpin_current_cpu+0x48/0x90
[11:16:24]** 2158 printk messages dropped ** [ 5.480233] SOFTE: 1

Labels (1)
0 Kudos
4 Replies

7,917 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello zhiming qiu,

It seems that this problem has already been fixed in SDK 2.0 1701 release.

I built RT Kernel as the following configuration in SDK 2.0 1703 build environment, I didn't reproduce your problem on B4860QDS.

Kernel options --->
        Preemption Model (Fully Preemptible Kernel (RT)) --->
                    (X) Fully Preemptible Kernel (RT)

Would you please try whether your problem remains with my Kernel uImage, I uploaded as the following.

https://drive.google.com/open?id=1vG9NUAlxgEA3JjKwbb19x-wKNc6LqIpe

Thanks,

Yiping

0 Kudos

7,917 Views
zhimingqiu
Contributor I

hello Yiping Wang,

 

Thanks for your reply。As you mentioned above,I have checked my config which is same with you . can you offer the .config file and the Modification instructions for  this problem in SDK 2.0 1701 to me?  

PS:The above problems need to be restarted many times;

0 Kudos

7,917 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached Kernel configuration file.

0 Kudos

7,917 Views
zhimingqiu
Contributor I

hello Yiping Wang,

I compared your configuration with mine.we find :  When we disabled the following options,The above problems did not appear in 24 hours;howerver,I need to use the following options in my project. You can test this problem by enabling the following options. Looking forward to your reply again.2019-10-25_103705.png2019-10-25_103722.png

Thanks,

0 Kudos