The first cmd8 interaction is out of time.LS1023

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The first cmd8 interaction is out of time.LS1023

1,806件の閲覧回数
weizhao_z
Contributor I

Now we are debugging the emmc.and the CPU used is ls1023.

the emmc model is mtfc8gacaa-4m.uboot is printed as follows.

It seems that the first cmd8 interaction is out of time.

sad.bmp

the schematic diagram is as follows.

RCW also the correct configurationqwe.bmp

anyone can help me ,please

thank u

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,557件の閲覧回数
Pavel
NXP Employee
NXP Employee

Your message dump shows the ETIMEDOUT error. See the errno.h file in the attachment. This error happens from mmc_send_cmd function (file mmc.c). It result from sdhci_send_command function from the sdhci.c file.

 

Check your board using the AN5012 LS1043a Design Checklist:

https://www.nxp.com/webapp/Download?colCode=AN5012&location=null&fsrch=1&sr=1&pageNum=1&Parent_nodeI...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,557件の閲覧回数
weizhao_z
Contributor I

emmm,

anyone have a similar problem?

0 件の賞賛
返信