The first cmd8 interaction is out of time.LS1023

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The first cmd8 interaction is out of time.LS1023

1,833 Views
weizhao_z
Contributor I

Now we are debugging the emmc.and the CPU used is ls1023.

the emmc model is mtfc8gacaa-4m.uboot is printed as follows.

It seems that the first cmd8 interaction is out of time.

sad.bmp

the schematic diagram is as follows.

RCW also the correct configurationqwe.bmp

anyone can help me ,please

thank u

Labels (1)
0 Kudos
Reply
2 Replies

1,584 Views
Pavel
NXP Employee
NXP Employee

Your message dump shows the ETIMEDOUT error. See the errno.h file in the attachment. This error happens from mmc_send_cmd function (file mmc.c). It result from sdhci_send_command function from the sdhci.c file.

 

Check your board using the AN5012 LS1043a Design Checklist:

https://www.nxp.com/webapp/Download?colCode=AN5012&location=null&fsrch=1&sr=1&pageNum=1&Parent_nodeI...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,584 Views
weizhao_z
Contributor I

emmm,

anyone have a similar problem?

0 Kudos
Reply