Need suggestion about B4860 vdd power supply.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need suggestion about B4860 vdd power supply.

2,214 Views
diankuixu
Contributor I

B4860 vdd is 1V, 38A, programmable (0.9~1.15V), is there some power chip used in B4860   suggested? price/easy to buy.

thanks a lot.

Labels (1)
0 Kudos
3 Replies

1,973 Views
diankuixu
Contributor I

Yes, on the demo board , Zy8160G used with ZM7304G( prodeced by POWER_ONE now is Bel Power Solutions, and I could not find it on Bel Power Solutions's web, and ZM7304G is expensive .)

So, it there some power chip better suggested?

Thanks a lot.

0 Kudos

1,973 Views
ufedor
NXP Employee
NXP Employee

Please consider that this area of the Community is devoted to the processors and it will be more convenient to ask the question in a power supplies area.

0 Kudos

1,973 Views
ufedor
NXP Employee
NXP Employee

ZY8160G is used on the B4860DS board.

0 Kudos