Is it possible to run more than one USDPAA application at once?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to run more than one USDPAA application at once?

跳至解决方案
1,656 次查看
jorhai
Contributor II

I notice that the USDPAA "dma_mem" driver prevents more than one USDPAA application running in the same time.

But we have to add USDPAA to multi-process. Is it possible?

标签 (1)
0 项奖励
回复
1 解答
1,394 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello sf dong,

It is possible to run multiple USDPAA applications at the same time, please make sure they use different buffer pools.

You need to modify the dts file to make different applications to use different Ethernet ports which use different buffer pools.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,395 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello sf dong,

It is possible to run multiple USDPAA applications at the same time, please make sure they use different buffer pools.

You need to modify the dts file to make different applications to use different Ethernet ports which use different buffer pools.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,394 次查看
jorhai
Contributor II

Hi Yiping.

          Thanks for your kindly reply.

          I will try it.

          But it is using the same DMA_mem while  seeding different buffer pools in multiple USDPAA applications. Will it cause overlay to memory.

          Thanks again.

           dongsf.

0 项奖励
回复