Can anybody share the i2c2 user guide for the bsc9132qds?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can anybody share the i2c2 user guide for the bsc9132qds?

771件の閲覧回数
manjanagoudapat
Contributor III


wusdk has the user manual for i2c on the bsc9131rdb. but i need the i2c user manual for bsc9132qds as the i2c2 interface is complex.

thanks and regards

patil

ラベル(1)
0 件の賞賛
返信
1 返信

639件の閲覧回数
Pavel
NXP Employee
NXP Employee

The BSC9132QDS driver is common I2C Linux driver.

Look at the following pages for I2C using under Linux:

https://xgoat.com/wp/2007/11/11/using-i2c-from-userspace-in-linux/

http://www.haifux.org/lectures/258/gpio_spi_i2c_userspace.pdf

https://www.kernel.org/doc/Documentation/i2c/dev-interface

http://elinux.org/Interfacing_with_I2C_Devices


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信