Hi Sir,
we are designing an switch with P1022 chip,and we plan to boot from SPI flash.So when build boot,we use commands like this:
make ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux-gnuspe- P1022DS_SPIFLASH_config
unset LDFLAGS
make ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux-gnuspe-
Then u-boot.bin will be built in the root dir.But after bure it to spi flash,and power on ,we found that cpu can't boot from spi flash.After searching from the internet,we got to know that PBI and RCW will be needed together with u-boot.bin to generate the final file.So could you please kindly attach the boot_format and the related config_sram.dat file for us?
Or please tell me how to get the tools and the config files ,thanks a lot .
Appreciate for your help.
解決済! 解決策の投稿を見る。
The requested files could be downloaded from the public git:
Dear sir,
Could you please help on this ?
After I got the spi image file and burn it on spi flash,I can not get any info from the console,I'm sure the cfg_rom_loc was set to :0110.
Is there anything I missed?Or something wrong with my operation?
Many thanks for that,have a good day!
Thanks
Jason
The requested files could be downloaded from the public git:
Hi sir,
Thanks for your kindly and professional help.
This is the boot code I used :fsl-sdk-v1.6-fb1-4.0
This is the steps I built u-boot.bin(Please help to check whether it‘s right or not’):
make ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux-gnuspe- P1022DS_SPIFLASH_config
unset LDFLAGS
make ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux-gnuspe-
After these done,I got u-boot.bin like this:482552 May 16 19:01 u-boot.bin
Copy the u-boot.bin to boot_format dir,and run:./boot_format config_ddr3_2gb_p1022ds.dat u-boot.bin -spi spi-uboot.bin,then got spi-uboot.bin like this:483840 May 16 18:28 spi-uboot.bin
But I found that other spi flash image was about 584K size,like u-boot-spi-P1022DS_SPIFLASH-2013.10+fslgit-r0.bin file
I burn spi-uboot.bin to spi flash,but can not see any info from my console
So what I need to confirm is :
1、Is it right for my steps to build u-boot.bin and spi-uboot.bin?
2、Why is the image size so strange?
3、If it‘s ok for my operation,do I have to modify user code size for file config_ddr3_2gb_p1022ds.dat ?
Thanks a lot!
Jason