real-time-edge build for i.MX93-EVK extensible SDK build fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

real-time-edge build for i.MX93-EVK extensible SDK build fails

3,021 Views
Z2025121
Contributor II

real-time-edge v2.9 for i.MX93-EVK

"bitbake nxp-image-real-time-edge" finished successfully

"bitbake nxp-image-real-time-edge -c populate_sdk_ext" fails

extensible SDK fails:

ERROR: The file /usr/include/ecrt.h is installed by both igh-ethercat and igh-ethercat-userspace, aborting

Any idea to fix the issue?

0 Kudos
Reply
3 Replies

2,932 Views
Z2025121
Contributor II

Hi,

Normal SDK does not have any build issue. But the extensible SDK "bitbake nxp-image-real-time-edge -c populate_sdk_ext"

fails because of a dependency issue: "/usr/include/ecrt.h is installed by both igh-ethercat and igh-ethercat-userspace". Is there any fix or workaround for the issue?

Many thanks.

BR

0 Kudos
Reply

2,999 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Have you tried using normal SDK first?
Does it have the same issues?

Best regards/Saludos,
Aldo.

0 Kudos
Reply

2,983 Views
Z2025121
Contributor II

The normal SDK does not have this build issue.

0 Kudos
Reply