package view not showing core elements from target MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

package view not showing core elements from target MCU

跳至解决方案
1,171 次查看
GMVS
Contributor III

Hi

i've got access to two computers with Code Warrior 10.2

in one of them (windows 7) the package view shows the MCU complete, with the core blocks and the pin names
but in the other (windows xp), it only says the name of the MCU without showing  core blocks, pin names, grounds, etc; it just shows the blanck green square there with the right name

does anyone knows how can i enable those features? because it doesnt shows them despite i change from MCU

 

thanks

0 项奖励
回复
1 解答
1,068 次查看
ProcessorExpert
Senior Contributor III

Hi,

the details are not visible in case the window is too small. Have you tried to use the magnifier glass icon :smileyplus: ?

 

best regards
Petr Hradsky
Processor Expert Support Team

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,069 次查看
ProcessorExpert
Senior Contributor III

Hi,

the details are not visible in case the window is too small. Have you tried to use the magnifier glass icon :smileyplus: ?

 

best regards
Petr Hradsky
Processor Expert Support Team

 

0 项奖励
回复