Hi,
I am using lpc54618 eval board, I was checking CLKOUT on oscilloscope using following code for BOARD_BootClockRUN but still was unable to see clock output on scope...
If I use :- CLOCK_AttachClk(kOSC32K_OSC_to_CLKOUT); /*!< Switch CLKOUT to OSC32K_OSC */
Or :- CLOCK_AttachClk(kMAIN_CLK_to_CLKOUT);
I get proper clkout on scope
I dont get output for :- CLOCK_AttachClk(kEXT_CLK_to_CLKOUT); /*!< Switch CLKOUT to EXT_CLK */
/*******************************************************************************
********************** Configuration BOARD_BootClockRUN ***********************
******************************************************************************/
/* clang-format off */
/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!Configuration
name: BOARD_BootClockRUN
called_from_default_init: true
outputs:
- {id: CLKOUT_clock.outFreq, value: 12 MHz}
- {id: FRO12M_clock.outFreq, value: 12 MHz}
- {id: FROHF_clock.outFreq, value: 48 MHz}
- {id: FXCOMs_CLK32K_clock.outFreq, value: 32.768 kHz}
- {id: MAIN_clock.outFreq, value: 12 MHz}
- {id: System_clock.outFreq, value: 12 MHz}
settings:
- {id: SYSCON.CLKOUTSELA.sel, value: SYSCON._clk_in}
sources:
- {id: RTC.rtc_32k_osc.outFreq, value: 32.768 kHz, enabled: true}
- {id: SYSCON._clk_in.outFreq, value: 12 MHz, enabled: true}
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* clang-format on */
/*******************************************************************************
* Variables for BOARD_BootClockRUN configuration
******************************************************************************/
/*******************************************************************************
* Code for BOARD_BootClockRUN configuration
******************************************************************************/
void BOARD_BootClockRUN(void)
{
/*!< Set up the clock sources */
/*!< Set up FRO */
POWER_DisablePD(kPDRUNCFG_PD_FRO_EN); /*!< Ensure FRO is on */
CLOCK_AttachClk(kFRO12M_to_MAIN_CLK); /*!< Switch to FRO 12MHz first to ensure we can change voltage without accidentally
being below the voltage for current speed */
POWER_DisablePD(kPDRUNCFG_PD_SYS_OSC); /*!< Enable System Oscillator Power */
SYSCON->SYSOSCCTRL = ((SYSCON->SYSOSCCTRL & ~SYSCON_SYSOSCCTRL_FREQRANGE_MASK) | SYSCON_SYSOSCCTRL_FREQRANGE(0U)); /*!< Set system oscillator range */
POWER_SetVoltageForFreq(12000000U); /*!< Set voltage for the one of the fastest clock outputs: System clock output */
CLOCK_SetFLASHAccessCyclesForFreq(12000000U); /*!< Set FLASH wait states for core */
/*!< Set up RTC OSC */
CLOCK_EnableClock(kCLOCK_Rtc); /*!< Enable the RTC peripheral clock */
RTC->CTRL &= ~RTC_CTRL_SWRESET_MASK; /*!< Make sure the reset bit is cleared */
RTC->CTRL &= ~RTC_CTRL_RTC_OSC_PD_MASK; /*!< Setup RTC oscillator */
SYSCON->RTCOSCCTRL = SYSCON_RTCOSCCTRL_EN_MASK; /*!< Setup RTC oscillator clock source availability to other modules */
/*!< Set up dividers */
CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 1U, false); /*!< Reset divider counter and set divider to value 1 */
CLOCK_SetClkDiv(kCLOCK_DivClkOut, 0U, true); /*!< Reset CLKOUTDIV divider counter and halt it */
CLOCK_SetClkDiv(kCLOCK_DivClkOut, 1U, false); /*!< Set CLKOUTDIV divider to value 1 */
/*!< Set up clock selectors - Attach clocks to the peripheries */
CLOCK_AttachClk(kFRO12M_to_MAIN_CLK); /*!< Switch MAIN_CLK to FRO12M */
CLOCK_AttachClk(kEXT_CLK_to_CLKOUT); /*!< Switch CLKOUT to EXT_CLK */
/* Set SystemCoreClock variable. */
SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK;
}
In Main function following code is used
{......
CLOCK_DisableClock(kCLOCK_ClockOut);
CLOCK_EnableClock(kCLOCK_ClockOut);
sourceClockFreq = CLOCK_GetClockOutClkFreq();
//CLOCK_SetClkDiv(kCLOCK_DivSpifiClk, sourceClockFreq / EXAMPLE_SPI_BAUDRATE - 1U, false);
CLOCK_SetClkDiv(kCLOCK_DivClkOut, sourceClockFreq / EXAMPLE_CLKOUT_BAUDRATE, false);
......}
Please let me know any suggestions or modifications to code to get CLKOUT from external crystal.