kl04.sct(7): error: L6236E: No section matches selector - no section to be FIRST/LAST.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kl04.sct(7): error: L6236E: No section matches selector - no section to be FIRST/LAST.

8,520件の閲覧回数
thoomanwang
Contributor V

Why?

0 件の賞賛
返信
5 返答(返信)

3,385件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

It seems that you are using Keil. Pleas add "--cpu Cortex-M0+" to the first line of the generated Scatter file of the ProcessorExpert (ProcessorExpert.scf). If the problems still exists, I think it is better also check with Keil support: http://www.keil.com/support/

0 件の賞賛
返信

3,385件の閲覧回数
thoomanwang
Contributor V

error.png

.\output\kl04.sct(7): error: L6236E: No section matches selector - no section to be FIRST/LAST.

kl04.sct file is keil own generated files, add - cpu Cortex-M0 + after invalid.

I use MDK4.7, support MKL04

0 件の賞賛
返信

3,385件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

could you please confirm that this issue was resolved within this thread: https://community.freescale.com/thread/308933

Or there still persist some issue?

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信

3,385件の閲覧回数
thoomanwang
Contributor V

In Iar 6.5 The problem has been resolved , but in the MDK4.7 in question , namely the question of this topic is still not resolved, but also invited experts to help solve

0 件の賞賛
返信

3,385件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Are you using CodeWarrior or Keil?

0 件の賞賛
返信