i.Mx7D Power management Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.Mx7D Power management Issue

635件の閲覧回数
sharmilad
Contributor I

Hi,

    We are using i.Mx7D for one of our custom project. We are trying to achieve the power management. We have 2 wakeup source. One is PIR interrupt (GPIO2_25) and another is WIFI interrupt (GPIO2_IO0).

We have configured both the interrupt as a wakeupsource from dts file. But we are observing "timeout waiting for hardware interrupt." error after system resumes from suspend. I have followed the below scenario 

1. Put the system into sleep using "echo mem > /sys/power/state" command.

2. Wakeup the system from wifi interrupt.   ----> No issue

3. Put the system into sleep

4. Wakeup the system using PIR ( sensor) interrupt. --->observed sdhci dump logs in the dmesg and system becomes unstable.

We are using Broadcom chipset for wifi.

I have attached my logs.

Please help me to resolve this issue

 

 

0 件の賞賛
3 返答(返信)

613件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Which kernel version are you working with?
Also, if wake up trough WiFi interrupt is working we can discard a hardware issue but just to be sure could you check with an oscilloscope when attempting wakeup from sensor interrupt?

Best regards,
Aldo.

0 件の賞賛

523件の閲覧回数
sharmilad
Contributor I

Hi,

Now I am successfully able to put the device into suspend mode and wakeup from gpio interrupt. My next concern is current consumption. In suspend mode my device is not reducing much current . And I could see pm-imx7.c and suspend-imx7.S file is not present in my arch/arm/mach-imx folder. Does these files are required for power management (suspend mode )? I am using kernel 5.10 version.

0 件の賞賛

500件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Glad to hear that you were successful with that, regarding consumption it would be difficult to say if its ok or not if I do not see the values for reference.

But you may take as reference based in the measurement we did back in the days for our EVK (AN5383), for “Suspend-To-RAM” in the Linux BSP. This is the lowest possible power state where the external supplies are still on.

Chapter 4.1.1 Deep-sleep mode (DSM)

AldoG_0-1687890780350.png


Also, please refer to this same App note chapter 5 Reducing Power Consumption for optimization on low power mode.

https://www.nxp.com/docs/en/application-note/AN5383.pdf

Best regards,
Aldo.

0 件の賞賛