how to fix your bugs, Processor Expert?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to fix your bugs, Processor Expert?

跳至解决方案
1,616 次查看
AndreiLuchuk
Contributor I

I found a bug where PE does not set the right registers. Can I fix this issue if I know the correct setting, or does it go into Notes? 

 

for example, I am using FTM2 on mc9s08pt60. Setting Edge Control to Rising/Falling should reflect in FTM2_C0SC[ELSB:ELSA] but its not, and I have to set it manually after init(). Is it a simple xml file which controls these setting, or is it more complex? 

 

As I understand it, PE is a complex tool, so bugs are bound to happen. What's Freescale's position on this? Is the user left to fend for themselves, or do we have an option other than a TSR? Thanks for your feedback!

0 项奖励
回复
1 解答
1,460 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

I think you will not be able to modify PEx driver directly (the files are encrupted), generaly your step with workaround in inti. was correct. In this case of existing workaround of the issue is the bug fixed in the next release.

 

However what I am missing in this issue is the following:

 

- version you use (CW + PEx) - please note in case you are using some older verison, there is possibility that the bug was already fixed in some newer version

 - could you please provide the project that leads you to getting the error

 

 

best regards
Vojtech Filip
Processor Expert Support Team

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,461 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

I think you will not be able to modify PEx driver directly (the files are encrupted), generaly your step with workaround in inti. was correct. In this case of existing workaround of the issue is the bug fixed in the next release.

 

However what I am missing in this issue is the following:

 

- version you use (CW + PEx) - please note in case you are using some older verison, there is possibility that the bug was already fixed in some newer version

 - could you please provide the project that leads you to getting the error

 

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复