Hi, I have a error when I add the component eeprom, the error says
+IEE1
+ERROR: Compiler option -CpPPAGE=0x15 (address of PPAGE register) or -CpPPAGE=RUNTIME must be set to compile the generated code correctly (current target settings, Compiler for HC12, Options, Code Generation tab, PPAGE register is used for paging). After compiler option change, run Code design to apply the change in Processor Expert. For details, see Help of the component.
+IEE1
+ERROR: There are errors in component, it is impossible to generate code
 
					
				
		
I do all steps, and still have the same error, thanks
 
					
				
		
Hello,
could you please provide the verison of PE and CW that you use?
best regards
Vojtech Filip
Processor Expert Support Team