does anyone have the flash on the TWR-K60F120M working using NFC_LDD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does anyone have the flash on the TWR-K60F120M working using NFC_LDD?

1,532 Views
bowerymarc
Contributor V

Is there any example code or anything?

I'm getting a problem reading the 64th block sequentially, NFC_LDD is returning with an ERR_BUSY...

anyone have code reading successfully reading/writing all the blocks of the Nand flash on this board (MT29F2G16ABAEAWP:E)

thx

M

Tags (2)
0 Kudos
Reply
4 Replies

1,283 Views
bowerymarc
Contributor V

followup - I realized that sometimes the flash operations return ERR_BUSY.  If I loop until the command doesn't return that, it seems to work.

So what's odd about that is, why is it busy?  I'm issuing commands one at a time, in a single thread, and waiting for the Done Interrupt to occur before issuing the next command.  Why would it return busy?

0 Kudos
Reply

1,283 Views
vfilip
NXP Employee
NXP Employee

Hello,

could you please send us (or post here) some demonstration project in order to reproduce it on our side?

Best regards

Vojtech Filip

Processor Expert Support Team

0 Kudos
Reply

1,283 Views
bowerymarc
Contributor V

the test code is in a larger project, which will be time consuming to unravel.  it would be simpler to send you the whole thing and tell you which function to look at, how to run it, and where to look for this issue, if that's OK?  If so I'll send it to you privately.  Otherwise it may take me a week or two to strip it down, based on my current workload.

0 Kudos
Reply

1,283 Views
vfilip
NXP Employee
NXP Employee

Hello,

please send the project on my email. It should be available in my profile.

Best regards

Vojtech Filip

Processor Expert Support Team

0 Kudos
Reply