about "code for component has not been generate yet"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about "code for component has not been generate yet"

ソリューションへジャンプ
1,851件の閲覧回数
LiKe
Contributor I

I use MQX3.8 add AD follow <<CW for Microcotrollers v10.x and MQX>> page 139. but I check AD and view source code.

the cw10.x POP "code for component has not been generate yet",why? bye the way, I use windows 7

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,641件の閲覧回数
ProcessorExpert
Senior Contributor III

Hi,

Could you please write more details on what CodeWarrior version are you using?

 

The Processor Expert code can be generated using the project pop-up menu command "Generate Processor Expert code" or you can use the icon (see attachment) in Processor Expert project panel. Processor Expert project panel can be opened using the command Window > Show view > Other... , select Processor Expert / Project panel.

 

best regards
Petr Hradsky
Processor Expert Support Team

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,642件の閲覧回数
ProcessorExpert
Senior Contributor III

Hi,

Could you please write more details on what CodeWarrior version are you using?

 

The Processor Expert code can be generated using the project pop-up menu command "Generate Processor Expert code" or you can use the icon (see attachment) in Processor Expert project panel. Processor Expert project panel can be opened using the command Window > Show view > Other... , select Processor Expert / Project panel.

 

best regards
Petr Hradsky
Processor Expert Support Team

 

 

 

0 件の賞賛
返信