This is a test, this is only a test, of file attachment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

This is a test, this is only a test, of file attachment

3,015 次查看
jimtrudeau
Senior Contributor I

We have a report of poor usability regarding attaching files. So I'm exploring.

I am creating a new topic, and at the bottom there is an Attach Files option and a Choose File button. That looks pretty easy. I'm attaching an old photo of a button "I Met MWRon" - this is a throwback to the old Metrowerks CodeWarrior days. MWRon was the guy who moderated/trolled all the internet forums for CodeWarrior issues. He was amazing.

So that looks easy enough. Next I'll try to reply and see how to attach a file to a reply.

0 项奖励
回复
2 回复数

2,667 次查看
jimtrudeau
Senior Contributor I

Ah, to reply, and attach a file, is not so easy. Here I am in the Reply interface, and there is the Add Reply button. But no obvious way to add a file.

The solution is to click the "Use Advanced Editor" button. All right. That solves the problem. In the "Advanced Editor" you get the "Choose File" button and all is right with the world.

I'm a believer in SINGULAR interfaces. Meaning that you should not see one interface when you start a thread, and a different one when you reply. No wonder people are confused. Unless there is really something radically different about starting a thread and replying to a message in a thread that already exists.

So, since this affects all communities, I can't promise instant change, we'll have to have a discussion here among the community owners. But let's see what we can do so that a Reply defaults to the Advanced editor and you can just as easily add a file to a reply as you can when starting a thread.

In the meantime, you can do two things.

1: When replying, click the Use Adanced Editor button - it's in the upper right

2: If you have already replied, Edit the reply.

0 项奖励
回复

2,665 次查看
jimtrudeau
Senior Contributor I

In celebration of Idiot UI problems, I thought I'd post one of my favorite images celebrating bad UI.

0 项奖励
回复