Hi, I am using TWR K60DN512 and code warrior 10.5. I have imported the PE code for Ethernet communication in the example list for twr k60DN512 board.It is working perfectly. The mac address given in the program is uint8_t MACAddress[] = { 0x06, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF }; but the device mac address written on the board is 00:04:9F:01:64:3B . when i tried to replace the mac address in the program with the mac address written on board the program is not receiving data back. Can anybody tell the reason? I need to establish an Ethernet communication interface. Which mac should i use? Thanks and regards Shiju