T4241 processor RESET_REQ_B signal probe output looks like continous pulses

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T4241 processor RESET_REQ_B signal probe output looks like continous pulses

跳至解决方案
2,121 次查看
kumar_086
Contributor IV

Dear Experts,

We are bringing up a T4241 processor board, loaded with RCW file in NOR Flash. In other boards we are able to see U-Boot booting.

In a particular board when we power on the board with UART, there is continuous character '' (triple bar) is printing on the terminal.

When we probed the processor signals its observed that signal 'RESET_REQ_B' output looks like a pulsed signal.

I'm new to this platform and requesting your help to resolve this.

Thanks

0 项奖励
回复
1 解答
2,099 次查看
r8070z
NXP Employee
NXP Employee

It is supposed that RESET_REQ signal triggers circuit which assigns PORESET (or HRESET). On reset RESET_REQ is negated and device tried to start. So we can imagine that toggling RESET_REQ signal means that during start due to some error device assigns RESET_REQ and as result is trying to start again and again. Possible reasons for RESET_REQ_B assertion you can find in the section “Reset Request Status Register (DCFG_CCSR_RSTRQSR1)” of the QorIQ T4240 Reference Manual. Probably Uboot image in the NOR flash has been damaged and device executes something wrong.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,746 次查看
kumar_086
Contributor IV

Thanks r8070z. After reprogramming Uboot image once again in NOR Flash, it's working now.

Regards!

0 项奖励
回复
2,100 次查看
r8070z
NXP Employee
NXP Employee

It is supposed that RESET_REQ signal triggers circuit which assigns PORESET (or HRESET). On reset RESET_REQ is negated and device tried to start. So we can imagine that toggling RESET_REQ signal means that during start due to some error device assigns RESET_REQ and as result is trying to start again and again. Possible reasons for RESET_REQ_B assertion you can find in the section “Reset Request Status Register (DCFG_CCSR_RSTRQSR1)” of the QorIQ T4240 Reference Manual. Probably Uboot image in the NOR flash has been damaged and device executes something wrong.

0 项奖励
回复