[T2080RDB] How to configure Common clock for PCIe endpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[T2080RDB] How to configure Common clock for PCIe endpoint

2,417 Views
Venkat_Vellanki
Contributor II

Hi,

We are working on T2080  PCIe . According to QorIQ_T2080_Reference_Manual(PgNo : 1545) we want to change the Common clock configuration(CCC) bit value in Link Control Register.

Can I get  more information on how to configure it in U-boot level?

image.png

Thanks and Regards,

Venkat Vellanki.

0 Kudos
Reply
5 Replies

2,340 Views
yipingwang
NXP TechSupport
NXP TechSupport

You can change the link control register in drivers/pci/fsl_pci_init.c

for ex as below to change cc to 1:

pci_lcr = pcie_cap_pos + 0x10;
temp32 |= 0x40;
pci_hose_write_config_dword(hose, dev, pci_lcr, temp32);

0 Kudos
Reply

2,332 Views
Venkat_Vellanki
Contributor II

Hi yipingwang  ,

Thanks for the response 

We have already changed as mentioned above but still couldn't configure to common clock.

We configured in the following path /drivers/pci/fsl_pci_init.c


void fsl_pci_init(struct pci_controller *hose, struct fsl_pci_info *pci_info)
{
#code
if (retrain_link_g)
{
pci_lcr = pcie_cap_pos + 0x10;
temp32 = 0;
pci_hose_read_config_dword(hose, dev, pci_lcr, &temp32);
printf("pci_lcr: 0x%x\n", temp32);
temp32 |= 0x40;
printf("pci_lcr mk: 0x%x\n", temp32);
pci_hose_write_config_dword(hose, dev, pci_lcr, temp32);
udelay(100000);
}
}

 

Are there any other modifications that are required.?

0 Kudos
Reply

2,351 Views
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 Kudos
Reply

1,984 Views
Venkat_Vellanki
Contributor II

Hi @yipingwang 

Please let us know any update on this as soon as possible .

 

Thanks,

Venkat Velanki.

 

Tags (1)
0 Kudos
Reply

1,976 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following update from the AE team.

No further information from software team since it is an old part with old SDK.
customer may search the source code and find a better way on their own.

0 Kudos
Reply