Goodmorning to All
I'm developing on K20 uP (MK20DN512VLL0) on KDS 2.0.0 and I have configurated some pin-
Now I try to configure 4 pin in a BitsIO_LDD (The module for set more than 1 pin)I s
Pin are: from 42 to 45 (PTA12 to PTA15)
I set port PTA, Output and 4 pins
I select the for pin but PE give me this error:
Description | Resource | Path | Location | Type |
Pin number differs from requested value: 5 (Pin) | UTe-Q | AnalogInput_Selection/Pin | Processor Expert Problem |
It is a very strange error...
What it means?
What I can do to solve it?
Many Thanks,
Massimiliano
已解决! 转到解答。
Hi,
The BitsIO_LDD component is used to configure consecutive pins as GPIO, you need to set 4 pins in the Pins field and configure consecutive pins in the tree. Here is the configuration I did fro your reference:
The consecutive bits PTA12 to PTA15 are configured as Inputs (GPIO).
You can find more information about the BitsIO_LDD component in the component user guide
<install_dir>\KDS_2.0.0\eclipse\ProcessorExpert\Help\ComponentUserGuides
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
The BitsIO_LDD component is used to configure consecutive pins as GPIO, you need to set 4 pins in the Pins field and configure consecutive pins in the tree. Here is the configuration I did fro your reference:
The consecutive bits PTA12 to PTA15 are configured as Inputs (GPIO).
You can find more information about the BitsIO_LDD component in the component user guide
<install_dir>\KDS_2.0.0\eclipse\ProcessorExpert\Help\ComponentUserGuides
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------