SDRAM: IS42S16100H-6TLI not working with IMXRT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM: IS42S16100H-6TLI not working with IMXRT1064

Jump to solution
1,523 Views
rajendrac4u
Contributor II

Hi All,

I need support for configuration the SEMC controller for the SDRAM access. Below is the controller and SDRAM we are using and you can find the schematic below.

Microcontroller : MIMXRT1064CVJ5B

SDRAM:  IS42S16100H-6TLI from Integrated Silicon Solution, Inc. (ISSI)

 

================================================================

code :

semc_config_t config;
semc_sdram_config_t sdramconfig;
uint32_t clockFrq = EXAMPLE_SEMC_CLK_FREQ;

/* Initializes the MAC configure structure to zero. */
memset(&config, 0, sizeof(semc_config_t));
memset(&sdramconfig, 0, sizeof(semc_sdram_config_t));

/* Initialize SEMC. */
SEMC_GetDefaultConfig(&config);
config.dqsMode = kSEMC_Loopbackdqspad; /* For more accurate timing. */
SEMC_Init(SEMC, &config);

/* Configure SDRAM. */
sdramconfig.csxPinMux = kSEMC_MUXCSX0;
sdramconfig.address = 0x80000000;
sdramconfig.memsize_kbytes = 2 * 1024; /* 32MB = 32*1024*1KBytes*/
sdramconfig.portSize = kSEMC_PortSize8Bit;
sdramconfig.burstLen = kSEMC_Sdram_BurstLen4;
sdramconfig.columnAddrBitNum = kSEMC_SdramColunm_8bit;
sdramconfig.casLatency = kSEMC_LatencyThree;
sdramconfig.tPrecharge2Act_Ns = 18; /* Trp 18ns */
sdramconfig.tAct2ReadWrite_Ns = 18; /* Trcd 18ns */
sdramconfig.tRefreshRecovery_Ns = 67; /* Use the maximum of the (Trfc , Txsr). */
sdramconfig.tWriteRecovery_Ns = 12; /* 12ns */
sdramconfig.tCkeOff_Ns =
42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/
sdramconfig.tAct2Prechage_Ns = 42; /* Tras 42ns */
sdramconfig.tSelfRefRecovery_Ns = 67;
sdramconfig.tRefresh2Refresh_Ns = 60;
sdramconfig.tAct2Act_Ns = 60;
sdramconfig.tPrescalePeriod_Ns = 160 * (1000000000 / clockFrq);
sdramconfig.refreshPeriod_nsPerRow = 64 * 1000000 / 8192; /* 64ms/8192 */
sdramconfig.refreshUrgThreshold = sdramconfig.refreshPeriod_nsPerRow;
sdramconfig.refreshBurstLen = 1;
return SEMC_ConfigureSDRAM(SEMC, kSEMC_SDRAM_CS0, &sdramconfig, clockFrq);
}

================================================================

Issue:

I am writing 1 to 200 from starting location 0x8000_0000 continuously.

when writing to the location 0x8000_0200 will also overwrite the the address 0x8000_0000.

similarly writing to address 0x8000_2001 will overwrite the the address 0x8000_0004 it will continue.

please let me the issue with my configuration or schematic.

I am using the SDK procided sdk project "evkmimxrt1064_semc"

rajendrac4u_0-1659609829201.png

rajendrac4u_2-1659609872811.png

 

 

0 Kudos
1 Solution
1,466 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Another thing worth noting is the use of the bit field BANK2 from the SDRAM Control Register 0. This bit should be set when the SDRAM device has 2 banks, which in this case it does. It is not fully implemented on the SDK example by default, but adding the BANK2 macro on the SEMC configuration would do it (fsl_semc.c):

base->SDRAMCR0 = SEMC_SDRAMCR0_PS(config->portSize) | SEMC_SDRAMCR0_BL(config->burstLen)  | SEMC_SDRAMCR0_COL(config->columnAddrBitNum) | SEMC_SDRAMCR0_CL(config->casLatency) | SEMC_SDRAMCR0_BANK2_MASK;

EdwinHz_0-1660362447977.png

This is image is from Application Note: AN12240

View solution in original post

0 Kudos
6 Replies
1,467 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Another thing worth noting is the use of the bit field BANK2 from the SDRAM Control Register 0. This bit should be set when the SDRAM device has 2 banks, which in this case it does. It is not fully implemented on the SDK example by default, but adding the BANK2 macro on the SEMC configuration would do it (fsl_semc.c):

base->SDRAMCR0 = SEMC_SDRAMCR0_PS(config->portSize) | SEMC_SDRAMCR0_BL(config->burstLen)  | SEMC_SDRAMCR0_COL(config->columnAddrBitNum) | SEMC_SDRAMCR0_CL(config->casLatency) | SEMC_SDRAMCR0_BANK2_MASK;

EdwinHz_0-1660362447977.png

This is image is from Application Note: AN12240

0 Kudos
1,446 Views
rajendrac4u
Contributor II

@EdwinHz 

Hello EdwinHz,

Thanks for the support, i am able to access the SDRAM memory properly now.

 

0 Kudos
1,513 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @rajendrac4u,

I believe the Bank Address Bits might be erroneous. The IS42S16100H’s Bank Address pin (A11) should be connected to SEMC_BA0 (GPIO_EMC_21) in order to properly differentiate between memory banks.

 

BR,

Edwin

0 Kudos
1,498 Views
rajendrac4u
Contributor II

Hello @EdwinHz 

Thanks for the reply.

I have done the changes suggested by you. Connected SEMC BA0 to SDRAM A11 pin.

now i am able to write from address 0x8000_0000 to 0x8000_0400.

after that it will overwrite from 0x8000_0000.

can you please help me.

rajendrac4u_0-1660126070085.png

Thanks 

Rajendra

0 Kudos
1,485 Views
EdwinHz
NXP TechSupport
NXP TechSupport

From the code snippet you attach, I see the port size was kept at 8 bits, considering that the IS42S16100 is a 16 bit SDRAM, I believe this should also be changed, since the whole address map changes according to the port size bit:

EdwinHz_2-1660248299316.png

 

EdwinHz_3-1660248299317.png

 

 

0 Kudos
1,479 Views
rajendrac4u
Contributor II

Hello @EdwinHz 

 

Sorry , we have updated the above code with 16bit , but still result is same.

0 Kudos