RTC programed to the wrong time by PE_LDD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC programed to the wrong time by PE_LDD

1,736 Views
randenewberry
Contributor IV

How can we stop PE_LDD from overwriting the time in the RTC registers with the values in the PE properties panel on Power up?

Using MK22FX512VLH12 with KDS.

0 Kudos
Reply
3 Replies

1,561 Views
mjbcswitzerland
Specialist V

Hi Rande

I don't know the PE generated code but I expect that you can simply add a check of the validity of the timer and abort any initialistion (which should only be done when it is has not yet been configured)

if ((RTC_SR & RTC_SR_TIF) != 0) {

    return; // RTC is alread operating so ignore

}

Note however that you will still need to ensure that the clock gate is enabled to the RTC after each reset (and to be able to check its validity) so the code will in fact look more like (similar to the uTasker time management solution):

POWER_UP(6, SIM_SCGC6_RTC);

if ((RTC_SR & RTC_SR_TIF) != 0) {

    return; // RTC is alread operating so ignore

}

// Continue with the configuration...

Regards

Mark

Kinetis: µTasker Kinetis support

K22: µTasker Kinetis FRDM-K22F support / µTasker Kinetis TWR-K22F120M support

Time Management: http://www.utasker.com/docs/uTasker/uTasker_Time.pdf

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply

1,561 Views
randenewberry
Contributor IV

Thank you Mark for the reply. The problem is with PE, and we found a way

to make it work.

Thanks!

Rande Newberry

H-ITT, LLC, a Hyper-Interactive Teaching Technology Company

420 Shearer Blvd.-Cocoa, FL, 32922

PH: 888-322-0089

[email protected]

0 Kudos
Reply

1,561 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have provided answer on the same previous question, see Re: rtc resets at powerup.

Best Regards,

Marek Neuzil

0 Kudos
Reply