Processor Expert report Error "Property DDR_DATA is set to a custom value"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor Expert report Error "Property DDR_DATA is set to a custom value"

跳至解决方案
1,200 次查看
benoitmasse
Contributor III

Hi,

I got this error and the only info that I have is 

Description Resource Path Location Type
Property DDR_RATE is set to a custom value. LS2088ARDB-Ben1 PBL1 Problem

It is not very usefull.

I pass every section in Properties page but I did not find any custom value.

Screenshot from 2021-01-14 23-27-14.png

I attached the PBL binary file. Note I add .c to be able to upload it but it's a binary file.

Thanks

0 项奖励
回复
1 解答
1,187 次查看
yipingwang
NXP TechSupport
NXP TechSupport

1.From Component Inspector view, select Enable/disable error checking menu, and then choose Skip error checking option, as shown in the figure below. 

 

yipingwang_0-1610952732298.png

 

 

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,188 次查看
yipingwang
NXP TechSupport
NXP TechSupport

1.From Component Inspector view, select Enable/disable error checking menu, and then choose Skip error checking option, as shown in the figure below. 

 

yipingwang_0-1610952732298.png

 

 

 

 

0 项奖励
回复