PE V2.99 for HCS12X
It seems that PE include files set their own internal DATA_SEG with
"#pragma DATA_SEG_PrExpxyz_DATA"
The same goes for CODE_SEG.
CODE_SEG is restored to DEFAULT at the end of the include file,
which I believe is the correct clean up method
DATA_SEG however is not restored to DEFAULT
resulting in my own variables belonging to the PE data segment
and not to the DEFAULT segment which would be a reasonable assumption.
Assuming I am correct in my description above I will appreciate answers
from the PE staff, to the following questions:
* Why is the DATA_SEG is NOT restored at the end of the include files?
* Why are PE defined DATA_SEG names not visible in the prm file?
If I am incorrect in my description, please explain where my reasoning is at fault.
Thank you,
Anders J