PE USB_HOST_STACK sends only first 4 bytes of the packet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE USB_HOST_STACK sends only first 4 bytes of the packet

865件の閲覧回数
qweasd
Contributor I

Hello, I'm using KDS v3.2.0 and USB_HOST_STACK PE Component from USB Stack v4.1.1.

I'm making a project for a custom vendor device that has only 2 bulk pipes, IN and OUT. I have almost the same project in CodeWarrior without using ProcessorExpert and that project works fine. 

My problem is that PE USB Stack has 2 bugs on my side, and the main bug is that _usb_host_send_data function sends only first 4 bytes of the buffer. I debugged through the code and figured out that the problem function is USB_LDD_HostSendData (generated by PE) within khci.c file. And this is the main difference between KDS and CW projects - CW ones uses _usb_khci_atom_tr to send/receive data.

The second bug is that I can receive the data from the device, but cannot get received data size, it is always set to the buffer size. But this bug is not critical.

I tried to port _usb_khci_task function from CW project to KDS one, but without any success.

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)