Hi,
I have just installed Processor Expert 10.4 and loaded the project for the TWR-K60F120M that I have previously used with Processor Expert 10.3. I have not knowingly made any changes from the original except for the build options - Compiler, which is now IAR ARM C Compiler, and generated the files.
When I use the Generate Processor Expert Code in 10.4 I get the error message:
Generator: FAILURE: Unexpected status of script: Drivers\Common\PE_MisraEnableRules.prg, please contact Freescale support. bsp_twrk60f120m Cpu Processor Expert Problem
If I change the Processor Expert directory configuration back to the 10.3 folder it works OK.
Is this a bug in 10.4 or is there really a problem with the configuration that 10.3 didn't pickup?
Best regards,
Adrian.
已解决! 转到解答。
Hi,
Please find the hotfix for Processor Expert Driver Suite 10.4 attached to this issue, try it and let us know if it fixes the issues in your project.
The description and instructions are enclosed in the readme file within the package.
Best regards
Petr Hradsky
Processor Expert Support Team
Hi Adrian,
I started integrating the MQX-Lite(RTOS folder) which is generated with codeWorrior(for KL46Z) with KL46Z IAR project.
Can you please tell me how to get the "IAR ARM C compiler" option in the CodeWarrior10.5?(able to see only CodeWarrior C compiler and GNU C Compiler).
I selected the GNU C compiler and created the KL46Z project using CodeWarrior10.5 and copied the MQX-Lite folder into KL46Z IAR project ,while compiling the project with IAR IDE am getting build errors in boot.S and dispatch.S files.
Updating build tree...
boot.S
Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 39
Error[42]: Duplicate label:'.equ' C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 44
Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 44
Error[42]: Duplicate label:'.equ' C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 45
Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 45
Error[42]: Duplicate label:'.equ' C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 46
Error[40]: Bad instruction C:\Users\KL46Z\MQXLITE\psp\cortex_m\types.inc 46
how to resolve this compiler dependent error? any suggestions..
Thanks in advance.
Regards,
--Ram.
Hi Ram,
When I started the New - Processor Expert Project I kept stepping through the wizard and the last option is to select the Target Compiler where "IAR ARM C Compiler" is one of the options. Once I had the project I added the MQX Lite component.
If I start a New - Processor Expert MQX-Lite Project then I don't get that last option. Not sure if that is a bug or by design.
I can also change the compiler by selecting the Cpu:... under the Processors section of the project components and then select the Build Options tab in the Component Inspector.
If the IAR compiler option does not appear then I'm afraid I don't know how to add it.
Best regards,
Adrian.
Hi,
I haven't been able to reproduce such problem yet. Could you please attached (simplified) project or at least the ProcessorExpert.pe file with the components configuration?
Best regards
Petr Hradsky
Processor Expert Support Team
Petr,
Any luck with this??
Gregory T. Powanda
Senior Field Applications Engineer
Arrow Electronics, Inc.
3245 Old Frankstown Road
Pittsburgh, PA 15239-2909
Phone: 724-387-7052
Cell: 412-759-6452
gpowanda@arrow.com <mailto:gpowanda@arrow.com>
www.arrow.com <http://www.arrow.com>
Save the date! AUGUST 28th is Arrow University in Pittsburgh…
From: GREGORY POWANDA
Sent: Friday, April 11, 2014 11:45 AM
To: 'jive-257545902-bl5-2-8gxc@freescale.hosted.jivesoftware.com'
Subject: RE: - PE 10.4 Error in PE_MisraEnableRules.prg
Petr,
Please find the project attached…
. I created a new project, selected the processor and IAR and added the MQX component. When I try to generate the code files, I get the error,
Gregory T. Powanda
Senior Field Applications Engineer
Arrow Electronics, Inc.
3245 Old Frankstown Road
Pittsburgh, PA 15239-2909
Phone: 724-387-7052
Cell: 412-759-6452
gpowanda@arrow.com <mailto:gpowanda@arrow.com>
www.arrow.com <http://www.arrow.com>
Save the date! AUGUST 28th is Arrow University in Pittsburgh…
Hi,
Thank you, I have reproducted the problem and passed it to the development team for analysis. It's most probably a bug.
Sorry for an inconvenience, we'll try to prepare some solution for you as soon as possible.
Best regards
Petr Hradsky
Processor Expert Support Team
Thanks Petr,
I’ll look forward to the reply back from the development team….
Gregory T. Powanda
Senior Field Applications Engineer
Arrow Electronics, Inc.
3245 Old Frankstown Road
Pittsburgh, PA 15239-2909
Phone: 724-387-7052
Cell: 412-759-6452
gpowanda@arrow.com <mailto:gpowanda@arrow.com>
www.arrow.com <http://www.arrow.com>
Save the date! AUGUST 28th is Arrow University in Pittsburgh…
Hi Greg,
I was informed that the problem is being fixed. Unfortunatelly, there seems to be no workaround so we will prepare a hot-fix package which should be available in the beginning of the next week.
Best regards
Petr Hradsky
Processor Expert Support Team
Hi,
Please find the hotfix for Processor Expert Driver Suite 10.4 attached to this issue, try it and let us know if it fixes the issues in your project.
The description and instructions are enclosed in the readme file within the package.
Best regards
Petr Hradsky
Processor Expert Support Team
Thanks Petr. This appears to solve the problem. Unfortunately I don't have the original project anymore as I started afresh with all the Freescale stuff because I had hacked it about so much when trying things out. I am having some issues with USB MSD host and wanted to be sure it was not anything I had changed causing the problems.
I have now used the Processor Expert 10.4 on a cloned BSP and it seems to be working.
Best regards,
Adrian.
Petr,
Please find the project attached…
. I created a new project, selected the processor and IAR and added the MQX component. When I try to generate the code files, I get the error,
Gregory T. Powanda
Senior Field Applications Engineer
Arrow Electronics, Inc.
3245 Old Frankstown Road
Pittsburgh, PA 15239-2909
Phone: 724-387-7052
Cell: 412-759-6452
gpowanda@arrow.com <mailto:gpowanda@arrow.com>
www.arrow.com <http://www.arrow.com>
Save the date! AUGUST 28th is Arrow University in Pittsburgh…
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.
Wlodek_D.,
This is actually an issue with the IAR Compiler and not CodeWarrior so I think Adrian has placed this in the correct location.
I have another customer that has received the exact same error message when trying to build a processor expert project with IAR....?