NFC_LDD seems to ignore LUN in calculating total size?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC_LDD seems to ignore LUN in calculating total size?

928 Views
bowerymarc
Contributor V

it seems the total size calc doesn't account for multiple LUNS (see attached image) but total pages is OK.  Will this actually affect the functionality?

NFC set error3.png

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

792 Views
Petr_H
NXP Employee
NXP Employee

Hi,

Yes you are right. There is a bug in the Total memory size calculation. This value is for information only and is not used in generated code so as a workaround please ignore the displayed value.

We are sorry for an inconvenience, it will be fixed in the next releases. 

Thanks for the information.

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply

792 Views
vfilip
NXP Employee
NXP Employee

Hello,

you can find the hot-fix to this issue in this thread: NFC_LDD ECC asking for too many bytes?

Best regards

Vojtech Filip

Processor Expert Support Team

0 Kudos
Reply