Missing embedded components(pbl,dpaa,ddr,device tree etc.) on a QorIQ Configuration Suite Project!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Missing embedded components(pbl,dpaa,ddr,device tree etc.) on a QorIQ Configuration Suite Project!

跳至解决方案
18,779 次查看
eminkoc
Contributor I

Hello,

 

I have downloaded the QorIQ Configuration Suite plug-in to my CW PA 10.2.1  IDE and followed the instructions of a freescale video to create a QorIQ config. project but no empedded components appeared on the components library window so I coulnd't generate a Processor Expert code. Here is the image of my IDE4093_4093.JPGCapture.JPG

 

But the Components Library window should be look like this:

4095_4095.JPGCapture2.JPG

 

How can I get these components?

I have searched for days but I couldn't find out why it has no component or where can I find them.

 

Thanks in advance

 

Emin Koç

Original Attachment has been moved to: console.txt.zip

Original Attachment has been moved to: cweclipse-items.rar.zip

标签 (1)
0 项奖励
回复
1 解答
18,064 次查看
PetrKraus
NXP Employee
NXP Employee

The root cause of this issue has been identified. Processor Expert file decoding doesn't work well on machines with Turkish local settings - using Turkish character set.

A hot-fix solution is available.

The problem will be fixed in QCS 2.3.4 (22-May-13).

在原帖中查看解决方案

0 项奖励
回复
24 回复数
2,813 次查看
PetrKraus
NXP Employee
NXP Employee

Yes, the package seems to be correct and complete.

Another suggestion, please, try to create a new Eclipse workspace:

File >> Switch Workspace

0 项奖励
回复
2,813 次查看
eminkoc
Contributor I

I switched the workspace but didn't work.

0 项奖励
回复
2,813 次查看
eminkoc
Contributor I

You saw the error message on the problems window right? It's always there, never dissapear. (you can see it on the first screenshot above)

0 项奖励
回复
18,065 次查看
PetrKraus
NXP Employee
NXP Employee

The root cause of this issue has been identified. Processor Expert file decoding doesn't work well on machines with Turkish local settings - using Turkish character set.

A hot-fix solution is available.

The problem will be fixed in QCS 2.3.4 (22-May-13).

0 项奖励
回复