Missing embedded components(pbl,dpaa,ddr,device tree etc.) on a QorIQ Configuration Suite Project!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing embedded components(pbl,dpaa,ddr,device tree etc.) on a QorIQ Configuration Suite Project!

Jump to solution
18,347 Views
eminkoc
Contributor I

Hello,

 

I have downloaded the QorIQ Configuration Suite plug-in to my CW PA 10.2.1  IDE and followed the instructions of a freescale video to create a QorIQ config. project but no empedded components appeared on the components library window so I coulnd't generate a Processor Expert code. Here is the image of my IDE4093_4093.JPGCapture.JPG

 

But the Components Library window should be look like this:

4095_4095.JPGCapture2.JPG

 

How can I get these components?

I have searched for days but I couldn't find out why it has no component or where can I find them.

 

Thanks in advance

 

Emin Koç

Original Attachment has been moved to: console.txt.zip

Original Attachment has been moved to: cweclipse-items.rar.zip

Labels (1)
0 Kudos
Reply
1 Solution
17,632 Views
PetrKraus
NXP Employee
NXP Employee

The root cause of this issue has been identified. Processor Expert file decoding doesn't work well on machines with Turkish local settings - using Turkish character set.

A hot-fix solution is available.

The problem will be fixed in QCS 2.3.4 (22-May-13).

View solution in original post

0 Kudos
Reply
24 Replies
2,753 Views
PetrKraus
NXP Employee
NXP Employee

Yes, the package seems to be correct and complete.

Another suggestion, please, try to create a new Eclipse workspace:

File >> Switch Workspace

0 Kudos
Reply
2,753 Views
eminkoc
Contributor I

I switched the workspace but didn't work.

0 Kudos
Reply
2,753 Views
eminkoc
Contributor I

You saw the error message on the problems window right? It's always there, never dissapear. (you can see it on the first screenshot above)

0 Kudos
Reply
17,633 Views
PetrKraus
NXP Employee
NXP Employee

The root cause of this issue has been identified. Processor Expert file decoding doesn't work well on machines with Turkish local settings - using Turkish character set.

A hot-fix solution is available.

The problem will be fixed in QCS 2.3.4 (22-May-13).

0 Kudos
Reply