MX8MN: Thermal driver doesn`t report temperatures below 10 degree celcius

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX8MN: Thermal driver doesn`t report temperatures below 10 degree celcius

ソリューションへジャンプ
2,163件の閲覧回数
MikeEngel
Contributor IV

Hi all,

using the Linux  kernel 5.4 and the MX8MN we have seen that when temperature drops below 10 degree celius the thermal driver report resource temporarily unavailable. 

In the source code of the driver (drivers/thermal/imx8mm_thermal.c) the following code will cause this behavior. 

if (tmu->socdata->flags == FLAGS_TMU_VER1) {
       val = readl_relaxed(tmu->base + TRITSR) & TRITSR_VAL_MASK;
       if (val < TEMP_LOW_LIMIT) {
               return -EAGAIN;
       }
}

Any explanation why the MX8MN has this low temperature limitation? 

Can this limitation be removed for industrial versions of the CPU?

Best regards,

--

Mike

0 件の賞賛
返信
1 解決策
2,140件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @MikeEngel ,

 

Based on IMX8MN Datasheet we have Temperature Sensor Accuracy set to 10-105 (Table 10. Operating ranges).

This is the reason of the limitation and it is applied in industrial products.

 

Regards,

Israel H.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,141件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @MikeEngel ,

 

Based on IMX8MN Datasheet we have Temperature Sensor Accuracy set to 10-105 (Table 10. Operating ranges).

This is the reason of the limitation and it is applied in industrial products.

 

Regards,

Israel H.

0 件の賞賛
返信
2,136件の閲覧回数
MikeEngel
Contributor IV

Thanks for this information. I found the data in the document you mentioned.

0 件の賞賛
返信