Dear all,
I'm developing a project based on the MCXA153VLH microprocessor.
It needs to sample an incoming analog voltage at regular intervals. I thought of using a timer to trigger the ADC to start the conversion.
I know that the ADC module of the MCXA153VLH microprocessor supports up to 4 hardware triggers, but I can't figure out the correspondence between the hardware peripheral and its specific trigger.
By analyzing the demo software provided with the SDK, I understand that Trigger 1 is associated with an IRQ generated by a pin. Which trigger is associated with a timer?
Thank you for your help and cooperation
regards
Hello @_Ferrari_
Sorry for replying to you late on this thread.
Fortunately, I have already answered this for you in your other thread.
If anyone else has the same issue, please refer to:
https://community.nxp.com/t5/MCX-Microcontrollers/MCXA153VLH-ADC-trigger/td-p/2155041
BR
Alice