[LS1028A]:How to enable SGMII PHY ethernet on ls1028a based board?.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LS1028A]:How to enable SGMII PHY ethernet on ls1028a based board?.

7,762件の閲覧回数
Amit_Keshri
Contributor III

Dear NXP Team,

We are using LS1028A based custom board and want to enable SGMII PHY ethernet which is connected to ls1028a processor as shown in attached schematic diagram.

I have set the RCW value as given below:

ENETC_RCW=3

SPI3_PMUX=0
GTX_CLK125_PMUX=1
SRDS_PLL_PD_PLL1=0
SRDS_PLL_PD_PLL2=1

Please find the below dts configuration for SGMI PHY ethernet:

/*-----------------------------------------------*/

&enetc_port1 {
phy-handle = <&sgmii_phy0>;
phy-connection-type = "sgmii";

mdio {
#address-cells = <1>;
#size-cells = <0>;
sgmii_phy0: ethernet-phy@0 {
reg = <0x0>;
};
};
};

&enetc_port0 {
status = "disabled";
};

&enetc_mdio_pf3 {

qsgmii_phy1: ethernet-phy@10 {
reg = <0x10>;
};

qsgmii_phy2: ethernet-phy@11 {
reg = <0x11>;
};
qsgmii_phy3: ethernet-phy@12 {
reg = <0x12>;
};

qsgmii_phy4: ethernet-phy@13 {
reg = <0x13>;
};
};


/* l2switch ports */
&mscc_felix_ports {
port@0 {
status = "okay";
phy-handle = <&qsgmii_phy1>;
phy-mode = "qsgmii";
managed = "in-band-status";
};

port@1 {
status = "okay";
phy-handle = <&qsgmii_phy2>;
phy-mode = "qsgmii";
managed = "in-band-status";
};
port@2 {
status = "okay";
phy-handle = <&qsgmii_phy3>;

/*-----------------------------------------------*/

In U-boot Ethernet is up and showing Alive as show in attached log ,after doing below configuration :

mii device emdio-3

mii write 0 0x16 0x12
mii write 0 0x14 0x8001

mii write 0 0x16 0x1
mii write 0 0x0 0x8140

mii write 0 0x16 0x0
mii write 0 0x0 0x8140

But in linux after setting ip address using ifconfig ,Ethernet is not pinging.

Please find all the required files i.e log ,schematic diagram for your reference.

Please tell me how i can enable SGNMII ethernet in linux?.

 

Regards,

Amit Kumar Keshri

 

0 件の賞賛
返信
3 返答(返信)

7,750件の閲覧回数
Amit_Keshri
Contributor III

Dear NXP Support Team,

Thank you for your reply

Regards,

Amit Kumar Keshri

0 件の賞賛
返信

7,752件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

7,721件の閲覧回数
Amit_Keshri
Contributor III

Dear NXP Support Team,

Eagerly Waiting for you reply.

Regards,

Amit Keshri

0 件の賞賛
返信