LS1028A 4port SGMII VSC8504

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A 4port SGMII VSC8504

Jump to solution
1,742 Views
junghunsung
Contributor I

Dear NXP experts.

I developing the custom board based on ls1028ardb board

and attached vsc8504 phy to ls1028a cpu.

the vsc8504 phy uboot driver is added on uboot/drivers/net/phy/vitesse.c

 <figure1> is block diagram, how to connect vsc8504 to cpu

<figure 1>

junghunsung_0-1670996556427.png

 

and ping test on uboot,

<figure2> is test configuration

junghunsung_3-1671001429344.png

 

Runnnig Wireshark on PC Side.

the custom board arp request packet is captured by wireshark 

and pc send reply packet, but custom board can't receive the reply

junghunsung_2-1671000627423.png

but sometimes  can receive about once in a hundred

Please refer and feedback.

what i should do?

 

 

===================== RCW ==========================

CLK_OUT_PMUX=0
63 ASLEEP_PMUX=0
64 RESET_REQ_PMUX=0
65 IIC1_PMUX=0
66 HOST_AGT_PEX1=0
67 HOST_AGT_PEX2=0
68 GP_INFO=0
69 EC1_SAI4_5_PMUX=0x1
70 EC1_SAI3_6_PMUX=0x1
71 USB_DRVVBUS_PMUX=1
72 USB_PWRFAULT_PMUX=1
73 USB3_CLK_FSEL=0x27
74 ENETC_RCW=0x3
75 SPI3_PMUX=0x1
76 GTX_CLK125_PMUX=1
77 SRDS_PLL_PD_PLL1=0
78 SRDS_PLL_PD_PLL2=1
79 /*
80 *SRDS_PRTCL_S1_L0=0x9
81 *SRDS_PRTCL_S1_L1=0x9
82 *SRDS_PRTCL_S1_L2=0x9
83 *SRDS_PRTCL_S1_L3=0x9
84 */
85 SRDS_PRTCL_S1_L0=9
86 SRDS_PRTCL_S1_L1=9
87 SRDS_PRTCL_S1_L2=9
88 SRDS_PRTCL_S1_L3=9
89 SRDS_PLL_REF_CLK_SEL_S1=0
90 SRDS_S1_REFCLK_SRC_SEL=0

 

===================== DTS ==========================

150 &mscc_felix_port0 {
151 label = "swp0";
152 phy-handle = <&sw_phy0>;
153 phy-mode = "sgmii";
154 status = "okay";
155 managed = "in-band-status";
156 };
157
158 &mscc_felix_port1 {
159 label = "swp1";
160 phy-handle = <&sw_phy1>;
161 phy-mode = "sgmii";
162 status = "okay";
163 managed = "in-band-status";
164 };
165
166 &mscc_felix_port2 {
167 label = "swp2";
168 phy-handle = <&sw_phy2>;
169 phy-mode = "sgmii";
170 status = "okay";
171 managed = "in-band-status";
172 };
173
174 &mscc_felix_port3 {
175 label = "swp3";
176 phy-handle = <&sw_phy3>;
177 phy-mode = "sgmii";
178 status = "okay";
179 managed = "in-band-status";
180 };
181
182 &mscc_felix_port4 {
183 ethernet = <&enetc2>;
184 status = "okay";
185 };
186
187 &mdio0 {
188 status = "okay";
189 /*
190 rdb_phy0: phy0 {
191 reg = <0>;
192 };
193 */
194 /* VSC8504 QSGMII PHY */
195 sw_phy0: phy@10 {
196 reg = <0x10>;
197 };
198 sw_phy1: phy@11 {
199 reg = <0x11>;
200 };
201
202 sw_phy2: phy@12 {
203 reg = <0x12>;
204 };
205
206 sw_phy3: phy@13 {
207 reg = <0x13>;
208 };
209 };

Tags (1)
0 Kudos
Reply
1 Solution
1,728 Views
junghunsung
Contributor I

it's solved

thanks

View solution in original post

0 Kudos
Reply
1 Reply
1,729 Views
junghunsung
Contributor I

it's solved

thanks

0 Kudos
Reply